[xen[domu]android hdmi/lvds output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[xen[domu]android hdmi/lvds output

238件の閲覧回数
Ahelion
Contributor IV

Hi experts,

I managed to boot-up Linux as Dom0 and android as DomU on my toradex verdin imx95.

Currently the linux has 2 screen outputs, one hdmi and one lvds. The android guest(android 14 trout) is displayed as a qemu window. 

How can I make android gain access to hdmi ( or lvds) so that linux has only one screen and android the other screen? I also want to route touch from the screen to the android when done. The problem is I do not know what to change. I have a feeling I need to change the device tree, but I am not sure how. Can anybody suggest a change that I can test?

Br, 

タグ(1)
0 件の賞賛
返信
1 返信

219件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, you have to put the setting in the device tree. Also contact @toradex for more issue with your board.

regards

 

0 件の賞賛
返信