writting magic word to safememory from linux based on the u-boot has to decide the bootmode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

writting magic word to safememory from linux based on the u-boot has to decide the bootmode

758件の閲覧回数
vadivelmurugan
Contributor I

Hi,

   Thank you in advance...

    I have queries on i.MX7d linux kernel, while user enter reboot command in linux console on i.MX7d during reboot time need to write some values like 0x12345678 in register or iram or some safememory, please suggest me the right way to write correct location.

  since I have written 0x00900000 and 0x00180000 location overwritten by u-boot.

Thanks 

Murugan R

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

711件の閲覧回数
vadivelmurugan
Contributor I

Hi,

 Thanks for your reply,

  I have tried the same , but it did not work out.

  Please suggest me anyother way to do warm reset and safeguard the data.

Regards

Murugan R

0 件の賞賛
返信

711件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Murugan

please look at SRC_GPR registers, described for example in

sect.6.2.7.24 SRC General Purpose Register 9 (SRC_GPR9)

i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信