working with i2c on imx6qp sabre ai board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

working with i2c on imx6qp sabre ai board

2,034 次查看
lavakumars
Contributor IV

hi,

I am working with the imx6qp sabre ai board. Trying to work on i2c device. on probing I can see no clock on the i2c bus. : Probed on "I2C2-SCL" signal can see no clock ticking can somebody help me?

Note: shorted all the places required for i2c2 bus.

Help me how to make i2c-2 bus to work.

current kernel version: 4.1.15.


Regards,

Lavakumar S

标记 (2)
0 项奖励
回复
6 回复数

1,820 次查看
b36401
NXP Employee
NXP Employee

Please enable i2c-2 in DTS file and rebuild the kernel.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,820 次查看
lavakumars
Contributor IV

hi Victor Linnik,

Thanks for the reply can you elaborate bit.. because I am new to this.

Regards,

Lava.

0 项奖励
回复

1,820 次查看
rajathks
Contributor II

Once you export the ARCH  and CROSS Compiler run "make menuconfig" .There you can configure you stuffs. and path it make the image

0 项奖励
回复

1,820 次查看
lavakumars
Contributor IV

hi rajath,

Thanks for replying . I tried menuconfig option there I can enable i2c interface ,its already enabled . but I want the i2c2 bus working that I couldn't see... if possible can you elaborate a bit please.

thanks & regards

Lavakumar S

0 项奖励
回复

1,820 次查看
rajathks
Contributor II

Well !! You are using your own customized DTS file or the Default one?

0 项奖励
回复

1,820 次查看
lavakumars
Contributor IV

default one only ... but I am not getting clock on i2c2 bus (i.e : i2c2_scl is pulled up no pulse).

0 项奖励
回复