I want to work SDMA with EIM on iMX6, but i didn't found that
anyone knows?
I'm using linux kernel 3.0.15
解決済! 解決策の投稿を見る。
OK, we only have one way : using SW to start SDMA.
Let me see how to !
Customers can send me email to ask for example code on how to use SDMA on WEIM interface !
At same time , Please provide project information.
Email : weidong.sun@freescale.com
From reference manual of i.mx6, in list of SDMA event mapping, no SDMA event for WEIM device. So external device connected to WEIM port can't trigger SDMA to work.
Dear Weidong Sun:
I want to implement use SDMA to transfer data mem to mem,Could you please send me a sample code.
My email: 863097177@qq.com
Thanks a lot!
does SDMA can support MEM to MEM transfer?
I think it's possible if SDMA can use mem to mem transfer.
Hello,Shin,
(1)does SDMA can support MEM to MEM transfer?
Yes, it is.
(2)I think it's possible if SDMA can use mem to mem transfer.
Yes, I think so.
(3)External device for WEIM
An external device on weim port should send a SDMA request to trigger or tell SDMA to begin to TX or RX. But in reference manual, this SDMA trigger for weim deive is not metioned.
Hello Weidong.
Could I also have the code for SDMA mem-to-mem transfers please? IF it makes any difference, I need internal to DDR3, and DDR3 back to internal.
Many thanks!
Mark.
I think SDMA trigger(TX,RX) can work by SW(program), not DMA request(external device event)
(2) MEM to MEM transfer
-> how can i use SDMA MEM to MEM transfer, my kernel source(linux 3.0.15) look like doesn't have mem to mem SDMA
script.
The Linux DMA APIs have been mapped to the SDMA.
The only thing you need to have is the Linux programming knowleadge.
In the Linux source tree, dmatest is the code for that.
https://community.nxp.com/thread/440728
OK, we only have one way : using SW to start SDMA.
Let me see how to !
Customers can send me email to ask for example code on how to use SDMA on WEIM interface !
At same time , Please provide project information.
Email : weidong.sun@freescale.com
hello,Weidong:
I am looking for some sample for data transfer with SDMA from WEIM-FPGA, platform is 3.14.28 , can
you send me the example?
my email: weid_vision@163.com
thanks a lot!
Hi @weidong_sun
I’m sorry for the sudden contact.
I need the sample code too. Please tell us how to get it.
Ko-hey
Hi weidong:
I'm working on transferring data over EIM from FPGA to imx6ul processor.
Could you send me the example code for testing?
Dear Weidong:
My email: baojianbin@owoncn.com
I want to transfer data using SDMA for WEIM-FPGA, Could you please send me the example code.
thanks !
Hello, Weidong. . I am currently studying with imx6q.
I will send you an email to see the next post by Weidong.
https://community.nxp.com/thread/304610
I need example on how to start SDMA with MEM to MEM mode.
A long time ago, but can you still give the sample source?
If possible, please reply to this email.
Thank you very much.
my email is kbs1439@sonartech.com
Dear Weidong:
Could you please send me the code of MEM TO MEM SDMA.
My email is: 421701136@qq.com
thanks a lot!
Hi Weidong:, could you also please send me the code for MEM to MEM SDMA. Email is akcooper8@gmail.com
I would appreciate getting your example code for doing memory <-> memory DMA using the WEIM bus.
My email is diebert@parc.com
Thank you,
Tim
Hello Weidong,
I want to use SDMA mem to mem transfer from shared memory from WEIM bus and internal or DDR3. Could you send me your example code ?
Thanks,
My email is philippe.verdier@oros.com
Hello Weidong,
I'm interrested in your example code of SDMA transfer on WEIM.
Please can you send it to me at mailto:bet.stf@gmail.com
Thank you
Dear Weidong:
I also want to test the mem to mem transfer using SDMA, Could you please send me the example code.
My email: sngik.lee@gmail.com
thanks a lot!
Hi Weidong,
Can you please send me the example code for SDMA for MEM to MEM transfer?
We are using the linux version : linux-3.0.35
My mail id :arun.krishna@sasken.com
Thanks in advance,
Arun Krishna
Hello,Shin,
Please tell me your Email address, Let me give you an example on how to start SDMA with MEM to MEM mode.
Regards,
Weidong