wlan0 interface is not coming up for onboard wifi module with imx8 Nano evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wlan0 interface is not coming up for onboard wifi module with imx8 Nano evk

4,961件の閲覧回数
shilesh_babu
Contributor II

Dear NXp,

As i am not able to bringing up the wifi module that is connected on imx8 Nano evk board, running below commands to bring up the interface, included wifi-tools to my .bblayer.

is there any other packages need to be add .bblayer to bring up this ?   

CMD outputs...

root@cu:~# ifconfig wlan0

ifconfig: wlan0: error fetching interface information: Device not found

root@cu:~# ifconfig wlan0 up
ifconfig: SIOCGIFFLAGS: No such device
Can not find device wlan0
ラベル(1)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,668件の閲覧回数
_angelo_
Contributor III

How is this wifi controlled ? In general

1 - check the interface, generally sdio, by dmesg, check the driver is up and device is detected.

2 - check finally ethernet driver fro wifi is running/loaded (lsmod)

3 - check for firmware load error messages, as   dmesg | grep err  or "dmesg | grep firm" and messahes around that

 

0 件の賞賛
返信

2,669件の閲覧回数
arrivederccimamasita
Contributor III

Hi everyone,

I'm having same issues in 2023  with the 8MNANOD4-EVK and the v6.1.1 Linux Distro version. I go through module activation with:

 

modprobe moal mod_para=nxp/wifi_mod_para.conf

After this, dmesg show:

Screenshot from 2023-06-19 17-00-56.png

Seems driver exists but its not  as verbose as i would like. Unfortunately, interface its not appearing

Screenshot from 2023-06-19 17-03-16.png

I tried to set the wifi network credentials in wpa_supplicant.conf and then updated with the command

wpa_supplicant -B -i wlan0 -c /etc/wpa_supplicant.conf -D nl80211

But seems not to brings up the interface

arrivederccimamasita_0-1687187229653.png

 

I tried this process with full and multimedia image in the application images provided. I also try v5-15.71 and v5.10.52, same results as above.

Someone have any idea what could be happening? Thanks!

0 件の賞賛
返信

4,854件の閲覧回数
romitchatterjee
Contributor V

Hi shilesh_babu,

You can check this post on the Murata forum: https://community.murata.com/s/question/0D55F000096S0K5SAK/imx-8m-nano-evk-wifi, which talks about a similar issue.

You can also refer to this Blog on the Murata forum: https://community.murata.com/s/article/Drill-down-Steps-to-Bring-up-1MW-on-i-MX8M-Mini-EVK. This describes the process of bring up the on-board Wi-Fi module on i.MX 8MMini. The procedure would be similar for 8MNano.

Best regards

0 件の賞賛
返信

4,911件の閲覧回数
shilesh_babu
Contributor II

Anyone have any update on the above question?

0 件の賞賛
返信

4,911件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the latest yocto release note, which Supports Murata 1MW (CYW43455) Wi-Fi/Bluetooth on i.MX 8M Mini and i.MX 8M Nano. so what WIFI module do you ues? and what bsp do you use

0 件の賞賛
返信