Hi, I'm integrating mender to imx93 evk and I'm hitting an issue that when I disable in u-boot CONFIG_ENV_IS_NOWHERE board hangs in SPL when flashing over uuu:
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x88000000, size 288
Download 1208320, Total size 1209344
NOTICE: BL31: v2.8(release):automotive-13.0.0_2.1.0-0-g99195a23d
NOTICE: BL31: Built : 11:12:16, Mar 28 2024
Any ideas why is this happening? I've tried to debug it but didn't find anything. When flash same image to SD card it boot without an issue. Thanks.