will imx8m evk board will support android automotive os?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

will imx8m evk board will support android automotive os?

1,589 Views
s_shridhar
Contributor II

how to enable android automotive os for imx8m evk board and what is the procedure for that?

what and all support is there for imx8m board?

Tags (2)
0 Kudos
Reply
3 Replies

1,543 Views
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately the i.MX8M it is a non Automotive device, so Andriod Auto, it is not in our development for i.MX8M  but we have the option for the i.Mx8Quad Max and the i.MX8X  which both devices are Automative Grade, the instructions or procedure for flashing an Android Auto, it is basically the same steps for a Regular Android Image.

0 Kudos
Reply

1,543 Views
s_shridhar
Contributor II

Hi jamesbone,

I have applied car patch for the android 9 pie source code then i have built and flashed on the imx8m evk board, now i am able to get the car functionalities , applications and services on the imx8m evk board, so is it supporting the android automotive?, can we get some car data through the vehicle hal to the kitchen sink application?

please clarify this.

893 Views
Imel
Contributor I

Hi @s_shridhar,

Could you provide some guidance or tutorial to do that, thank you in advance.

Best regards,

0 Kudos
Reply