wifi can not work normaly in L3.14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wifi can not work normaly in L3.14

1,789 Views
chengsi
Contributor I

Hi,

>>I am using bcm43438 in our customer imx7d board with Linux3.14.

The  wifi firmware I use is "brcmfmac43430-sdio.bin" and "brcmfmac43430-sdio.txt" from raspberry pi, when use "modprobe bcmdhd firmware_path=/lib/firmware/bcm/BCM43430/brcmfmac43430-sdio.bin nvram_path=/lib/firmware/bcm/BCM43430/brcmfmac43430-sdio.txt dhd_meg_level=0x1" i get the message:

dhd_module_init in
Power-up adapter 'DHD generic adapter'
wifi_platform_bus_enumerate device present 1
mmc0: new high speed SDIO card at address 0001
F1 signature OK, socitype:0x1 chip:0xa9a6 rev:0x1 pkg:0x4
DHD: dongle ram size is set to 524288(orig 524288) at 0x0
wifi_platform_get_mac_addr
CFG80211-ERROR) wl_setup_wiphy : Registering Vendor80211)
wl_create_event_handler(): thread:wl_event_handler:16e started
CFG80211-ERROR) wl_event_handler : tsk Enter, tsk = 0xa8d0141c
dhd_attach(): thread:dhd_watchdog_thread:16f started
dhd_attach(): thread:dhd_dpc:170 started
dhd_deferred_work_init: work queue initialized
dhdsdio_write_vars: Download, Upload and compare of NVRAM succeeded.
dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
wifi_platform_get_mac_addr
Firmware up: op_mode=0x0005, MAC=00:90:4c:c5:12:38
Firmware version = wl0: May 27 2016 00:13:38 version 7.45.41.26 (r640327) FWID 01-df77e4a7
dhd_wlfc_init(): successfully enabled bdcv2 tlv signaling, 79
dhd_wlfc_init: query wlfc_mode succeed, fw_caps=0x1c
dhd_wlfc_init(): wlfc_mode=0x1c, ret=0
Dongle Host Driver, version 1.141.72 (r)
Compiled from
Register interface [wlan0] MAC: 00:90:4c:c5:12:38
>>It seems the driver is loaded successfully, so I use try to start the wifi:
root#ifconfig wlan0 up
root#ifconfig
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1%1995585232/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:4 errors:0 dropped:0 overruns:0 frame:0
TX packets:4 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:240 (240.0 B) TX bytes:240 (240.0 B)
wlan0 Link encap:Ethernet HWaddr 00:90:4C:C5:12:38
inet6 addr: fe80::290:4cff:fec5:1238%1995585232/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:15 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:2778 (2.7 KiB)
>>so it seems the wifi module start correctly, but when i try to scan for AP, it get nothing:
root#iw dev wlan0 scan
root#
root#iwlist wlan0 scan
wlan0  Interface doesn't support scanning.
root#
>>here is my dts, please give me some advise, do I need modify the bdmdhd driver or change the firmware?
bcmdhd_wlan_0: bcmdhd_wlan@0 {
compatible = "android,bcmdhd_wlan";
/* WL_HOST_WAKE=GPIO<5,2>, WL_REG_ON=GPIO<5,1> */
gpios = <&gpio5 2 0>;
wlreg_on-supply = <&wlreg_on>;
};

regulators {
compatible = "simple-bus";
#address-cells = <1>;
#size-cells = <0>;

wlreg_on: fixedregulator@100 {
compatible = "regulator-fixed";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-name = "wlreg_on";
gpio = <&gpio5 1 0>;
startup-delay-us = <100>;
enable-active-high;
};
};
/*wifi*/
&usdhc1 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc1>;
pinctrl-1 = <&pinctrl_usdhc1_100mhz>;
pinctrl-2 = <&pinctrl_usdhc1_200mhz>;
cd-gpios = <&gpio7 6 GPIO_ACTIVE_HIGH>;
/*cd-post;*/
bus-width = <4>;
no-1-8-v;
enable-sdio-wakeup;
keep-power-in-suspend;
non-removable;
pm-ignore-notify;
wifi-host; 
status = "okay";
};
pinctrl_usdhc1: usdhc1grp {
fsl,pins = <
MX7D_PAD_SD1_CMD__SD1_CMD 0x59
MX7D_PAD_SD1_CLK__SD1_CLK 0x19
MX7D_PAD_SD1_DATA0__SD1_DATA0 0x59
MX7D_PAD_SD1_DATA1__SD1_DATA1 0x59
MX7D_PAD_SD1_DATA2__SD1_DATA2 0x59
MX7D_PAD_SD1_DATA3__SD1_DATA3 0x59
MX7D_PAD_SD1_WP__GPIO5_IO1 0x59
>;
};
0 Kudos
4 Replies

1,079 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cheng

one can try attached patch, but i.MX7D supported in L3.14.52 kernel with beta quality,

suggest to migrate to latest L4.1.xx kernels described on link

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,079 Views
chengsi
Contributor I

hi igorpadykov,

I have tried the patch, but the result is same,  when i use "iw dev wlan0 scan", it still get nothing , and i can not connect to any wifi.

As i can see, the firemware is named "brcmfmac", does it mean i should use brcmfmac driver?

0 Kudos

1,079 Views
igorpadykov
NXP Employee
NXP Employee

Linux 3.14 is very old kernel, for its support please apply to Murata support link
wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html
or use latest bsps described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor

0 Kudos

1,079 Views
chengsi
Contributor I

Hi  igorpadykov,

  I have tried the latest kernel 4.1.42 from freescale github, but the result is the same. when i try to scan for aps, it still return nothing, and can not connect to my ap.

   I think maybe the driver or the cmd i use is wrong or too old? 

0 Kudos