We are having problem with board that is based on imx6sl evk and rtl8192cu (chip on wifi module is RTL8188CTV). The wifi module is on USB interface.
We integrated rtl8192cu driver from another package, we used manual supplied by realtek to integrate there driver into android (from zip file RTL8188C_8192C_USB_linux_v4.0.2_9000.20130911.zip pdf file \android_ref_codes_JB_4.2\Realtek_Wi-Fi_SDK_for_Android_JB_4_2.pdf).
The driver is build as part of the kernel, not module. We used there's wpa_supplicant, that came with realteks package (wpa_supplicant_8_jb_4.2_rtw_r8680.20130821.tar.gz).
Package is from this site: http://www.realtek.com/downloads/downloadsView.aspx?Langid=2&PFid=48&Level=5&Conn=4&ProdID=277&DownT...
RTL8192CU for Linux/Android
Firmware is from this link: rtl819x - Linux Wireless
Using serial interface terminal, we tested the wlan0 interface, we can bring it up, and get ip number:
root@evk_6sl:/ # cat /sys/kernel/debug/usb/devices
T: Bus=02 Lev=01 Prnt=01 Port=00 Cnt=01 Dev#= 2 Spd=480 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS=64 #Cfgs= 1
P: Vendor=0bda ProdID=8176 Rev= 2.00
S: Manufacturer=Realtek
S: Product=802.11n WLAN Adapter
S: SerialNumber=00e04c000001
C:* #Ifs= 1 Cfg#= 1 Atr=a0 MxPwr=500mA
I:* If#= 0 Alt= 0 #EPs= 4 Cls=ff(vend.) Sub=ff Prot=ff Driver=rtl8192cu
E: Ad=81(I) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=02(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=03(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=84(I) Atr=03(Int.) MxPS= 64 Ivl=125us
root@evk_6sl:/ # dhcpcd wlan0
dhcpcd[2859]: version 5.5.6 start+871x_drv - drv_open, bup=0
===> FirmwareDownload91C() fw:Rtl819XFwImageArray_UMC_B
FirmwareDownload92C accquire FW from embedded image
fw_ver=v80, fw_subver=0, sig=0x88c0
fw download ok!
Set RF Chip ID to RF_6052 and RF type to 1T1R.
IQK:Start!!!
Path A IQK Success!!
Path A IQK Success!!
IQK: final_candidate is 0
IQK: RegE94=103 RegE9C=f RegEA4=fb RegEAC=5 RegEB4=0 RegEBC=0 RegEC4=0 RegECC=0
Path A IQ Calibration Success !
pdmpriv->TxPowerTrackControl = 1
MAC Address from REG_MACID = 44:33:4c:8b:f2:10
rtl8192cu_hal_init in 610ms
MAC Address = 44:33:4c:8b:f2:10
-871x_drv - drv_open, bup=1
ADDRCONF(NETDEV_UP): wlan0: link is not ready
dhcpcd[2859]: wlan0: checking for 169.254.169.141
dhcpcd[2859]: wlan0: using IPv4LL address 169.254.169.141
dhcpcd[2859]: forked to background, child pid 2885
root@evk_6sl:/ # ifconfig wlan0
wlan0: ip 169.254.169.141 mask 255.255.0.0 flags [up broadcast running multicast]
root@evk_6sl:/ # netcfg
lo UP 127.0.0.1/8 0x00000049 00:00:00:00:00:00
eth0 UP 192.168.0.152/24 0x00001043 24:80:00:00:00:00
tunl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
sit0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
ip6tnl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
wlan0 UP 169.254.169.141/16 0x00001043 44:33:4c:8b:f2:10
We need to use dhcpcd wlan0 command, the suggested init.rs service doesn't work, but thats not the problem.
Our problem is that binding from android ui and kernel isnt working.
When we tried to turn on wifi, from Settings>Wifi in Android UI, the slider button can move and change to On state, but the message on display "To see available networks, turn WiFi on" is still there.
in logcat we get:
D/WifiService( 2363): setWifiEnabled: true pid=2363, uid=1000
After that we can't move slider back.
When we exit that menu and return, the slider is back in Off state.
Using wifi from shell, we can get all the other wifi networks:
root@evk_6sl:/data # ./xbin/iwlist wlan0 scanning
survey done event(18)
wlan0 Scan completed :
Cell 01 - Address: BC:AE:C5:C4:3B:F7
ESSID:"Automatic"
Protocol:IEEE 802.11bg
Mode:Master
Frequency:2.412 GHz (Channel 1)
Encryption key:on
Bit Rates:54 Mb/s
Quality=59/100 Signal level=-95 dBm
Cell 02 - Address: 68:7F:74:01:C6:BE
ESSID:""
Protocol:IEEE 802.11bg
Mode:Master
Frequency:2.432 GHz (Channel 5)
Encryption key:off
Bit Rates:54 Mb/s
Quality=100/100 Signal level=-55 dBm
Cell 03 - Address: 20:AA:4B:1B:A1:7C
ESSID:"TEST"
Protocol:IEEE 802.11bgn
Mode:Master
Frequency:2.437 GHz (Channel 6)
Encryption key:off
Bit Rates:144 Mb/s
IE: Unknown: DD750050F204104A0001101044000102103B0001031047001020AA4B1BA17A20AA4B1BA17A022AC107102100104C696E6B73797320627920436973636F102300085752543136304E4C1024000776312E302E303210420001351054000800060050F2040001101100085752543136304E4C100800020084
Quality=100/100 Signal level=-71 dBm
Cell 04 - Address: 00:1D:7E:BD:10:05
ESSID:"alt02"
Protocol:IEEE 802.11bg
Mode:Master
Frequency:2.457 GHz (Channel 10)
Encryption key:on
Bit Rates:54 Mb/s
Extra:wpa_ie=dd180050f20101000050f20201000050f20201000050f2020c00
IE: WPA Version 1
Group Cipher : TKIP
Pairwise Ciphers (1) : TKIP
Authentication Suites (1) : PSK
Quality=100/100 Signal level=-74 dBm
Cell 05 - Address: 00:18:F8:3B:F1:0A
ESSID:"alt1"
Protocol:IEEE 802.11bg
Mode:Master
Frequency:2.462 GHz (Channel 11)
Encryption key:on
Bit Rates:54 Mb/s
Quality=101/100 Signal level=-95 dBm
We also added permissions for wifi in android ..
Please, ask me if you need more details, I kept track of all the changed done in the android and kernel.
Logcat with DBG for classes in wifi is also available.
Does anyone have any idea about this problem? Could you help us, please? We wasted a lot of time on this.
解決済! 解決策の投稿を見る。
Yes, we manage to get wifi working. Here are info's in more detail, so if anybody else has problem ...
We build driver as part of the kernel:
vim kernel_imx/arch/arm/configs/imx6s_{yourdevice}_android_defconfig
CONFIG_CFG80211=y
CONFIG_MAC80211_MESH=y
CONFIG_MAC80211=y
CONFIG_HOSTAP=y
CONFIG_RTL8192CU=y
CONFIG_RTLWIFI=y
CONFIG_RTL8192C_COMMON=y
#CONFIG_RTL8723AS=m
CONFIG_USB_USBNET=y
CONFIG_NET_RADIO=y
vim device/fsl/{yourdevice}/BoardConfig.mk
BOARD_WIFI_VENDOR := realtek
WPA_SUPPLICANT_VERSION := VER_0_8_X
CONFIG_DRIVER_NL80211 := true
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_WLAN_DEVICE := rtl8192cu
WIFI_DRIVER_MODULE_NAME := "wlan0"
WIFI_DRIVER_MODULE_PATH := ""
WIFI_DRIVER_MODULE_ARG := ""
WIFI_FIRMWARE_LOADER := ""
WIFI_DRIVER_FW_PATH_STA := ""
WIFI_DRIVER_FW_PATH_AP := ""
WIFI_DRIVER_FW_PATH_P2P := ""
WIFI_DRIVER_FW_PATH_PARAM := ""
We disabled p2p, since we dont need it:
vim device/fsl/imx6/{yourboard}.mk
PRODUCT_COPY_FILES += \
#frameworks/native/data/etc/android.hardware.wifi.direct.xml:system/etc/permissions/android.hardware.wifi.direct.xml
or
rm out/target/product/{yourboard}/system/etc/permissions/android.hardware.wifi.direct.xml
or just remount system partition:
root@{yourboard}:/ # mount -o remount, rw /system;
and remove xml:
root@{yourboard}:/ # rm /system/etc/permissions/android.hardware.wifi.direct.xml
edit:
root@{yourboard}:/ # busybox vi system/etc/permissions/required_hardware.xml
or
vim device/fsl/{yourboard}/required_hardware.xml
or
vim out/target/product/{yourboard}/system/etc/permissions/required_hardware.xml
<!--
<feature name="android.hardware.wifi.direct" />
-->
If you use it as module, you will need to add it also in PRODUCT_COPY_FILES
You need to correct init scripts, leave just this lines:
(this is from: http://blog.linuxconsulting.ro/2010/04/porting-wifi-drivers-to-android.html )
You can do it directly to out folder:
vim out/target/product/{yourboard}/root/init.rc
or/and (rebuild the whole system):
vim device/fsl/imx6/imx6.mk
mkdir /system/etc/wifi 0770 wifi wifi
chmod 0770 /system/etc/wifi
chmod 0660 /system/etc/wifi/wpa_supplicant.conf
chown wifi wifi /system/etc/wifi/wpa_supplicant.conf
#wpa_supplicant control socket for android wifi.c (android private socket)
mkdir /data/misc/wifi 0770 wifi wifi
mkdir /data/misc/wifi/sockets 0770 wifi wifi
chmod 0770 /data/misc/wifi
chmod 0660 /data/misc/wifi/wpa_supplicant.conf
chown wifi wifi /data/misc/wifi
chown wifi wifi /data/misc/wifi/wpa_supplicant.conf
setprop wifi.interface wlan0
setprop wlan.driver.status "ok"
#setprop wifi.ap.interface wlan0
#and also remove this lines:
# mkdir /data/system/wpa_supplicant 0771 wifi wifi
# chmod 0771 /data/system/wpa_supplicant
# symlink /data/misc/wifi/wpa_supplicant /data/system/wpa_supplicant
you can read it in that blog link, about unix/android standard socket setup.
vim out/target/product/{yourboard}/root/init.freescale.rc
or/and
vim device/fsl/{yourboard}/init.rc
#this is the only supplicant service and dhcpcd service for wifi that we use:
service rtw_suppl /system/bin/wpa_supplicant -dd -iwlan0 -Dnl80211 \
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class main
disabled
oneshot
service dhcpcd_wlan0 /system/bin/dhcpcd -aABKL
class main
disabled
oneshot
service iprenew_wlan0 /system/bin/dhcpcd -n
class main
disabled
oneshot
To keep it clean (it doesnt effect wifi):
vim device/fsl/imx6/imx6.mk
PRODUCT_PACKAGES += \
rtw_suppl \
We needed to make a little change in wifi_realtek.c since our jb is 4.3:
vim hardware/realtek/wlan/libhardware_legacy/wifi/wifi_realtek.c
int wifi_start_supplicant(int p2p_supported)
..
wifi_stop_supplicant(p2p_supported);
….
int wifi_stop_supplicant(int p2p_supported){
char supp_status[PROPERTY_VALUE_MAX] = {'\0'};
int count = 50; /* wait at most 5 seconds for completion */
if (p2p_supported) {
property_get("wifi.supplicant", supplicant_name, P2P_SUPPLICANT_NAME);
snprintf(supplicant_prop_name, PROPERTY_KEY_MAX, P2P_PROP_NAME, supplicant_name);
} else {
property_get("wifi.supplicant", supplicant_name, SUPPLICANT_NAME);
snprintf(supplicant_prop_name, PROPERTY_KEY_MAX, SUPP_PROP_NAME, supplicant_name);
}
Our problem was wrong supplicant name in prop setup. And, when wifi starts it first stops supplicant, and it wasn’t able to transfer that info through system. It was quite fun tracking this problem.
vim ./frameworks/base/wifi/java/android/net/wifi/WifiStateMachine.java
mWifiNative.killSupplicant(mP2pSupported);
if(mWifiNative.startSupplicant(mP2pSupported)) {
setWifiState(WIFI_STATE_ENABLING);
if (DBG) log("Supplicant start successful");
mWifiMonitor.startMonitoring();
transitionTo(mSupplicantStartingState);
} else {
loge("Failed to start supplicant!!");
}
Here are more info:
root@{yourdevice}:/ # cat /data/misc/wifi/wpa_supplicant.conf
ctrl_interface=wlan0
update_config=1
device_name={yourdevice}
manufacturer=Freescale
model_name={YOURDEVICE}
model_number={YOURDEVICE}
serial_number=
device_type=10-0050F204-5
config_methods=physical_display virtual_push_button
network={
ssid="XXXXX"
key_mgmt=NONE
priority=1
}
and it started with:
root@{yourdevice}:/ # cat system/etc/wifi/wpa_supplicant.conf
update_config=1
ctrl_interface=wlan0
eapol_version=1
ap_scan=1
fast_reauth=1
permissions:
root@{yourdevice}:/ # ls -l /data/misc/wifi
-rw-rw---- system wifi 21 2014-05-27 12:39 entropy.bin
drwxrwx--- wifi wifi 2014-05-27 12:39 sockets
-rw------- system system 33 2014-05-27 12:39 softap.conf
-rw-rw---- wifi wifi 272 2014-05-27 12:39 wpa_supplicant.conf
root@{yourboard}:/ # ls -l /data/misc/
drwxr-s--- system shell 2014-05-27 12:39 adb
drwxrwx--- bluetooth net_bt_stack 2014-05-27 12:39 bluedroid
drwxrwx--- system system 2014-05-27 12:39 bluetooth
drwxrwx--- dhcp dhcp 2014-05-27 12:39 dhcp
drwxrwx--x system system 2014-05-27 12:39 keychain
drwx------ keystore keystore 2014-05-27 12:39 keystore
drwx------ media media 2014-05-27 12:39 media
drwxrwx--- system radio 2014-05-27 12:39 radio
drwxrwx--- system radio 2014-05-27 12:39 sms
drwx------ system system 2014-05-27 12:39 systemkeys
drwxrwx--- system vpn 2014-05-27 12:39 vpn
drwxrwx--- wifi wifi 2014-05-27 12:39 wifi
drwxrwxr-x system system 2014-05-27 12:39 zoneinfo
root@{yourboard}:/ # ls -l /system/etc/wifi
-rw-rw---- wifi wifi 77 2014-05-27 12:39 wpa_supplicant.conf
root@{yourboard}:/ # ps | grep wpa
wifi 2555 1 3104 1876 c0103edc 401a4448 S /system/bin/wpa_supplicant
root@{yourboard}:/ # cat system/etc/permissions/platform.xml | grep -i wifi
<permission name="android.permission.ACCESS_WIFI_STATE" >
<group gid="wifi" />
<permission name="android.permission.CHANGE_WIFI_STATE" >
<group gid="wifi" />
<permission name="android.permission.WIFI" >
<group gid="wifi" />
root@{yourboard}:/ # cat system/etc/permissions/required_hardware.xml | grep wifi
<feature name="android.hardware.wifi" />
root@{yourboard}:/ # getprop | grep wifi
[net.tcp.buffersize.wifi]: [524288,1048576,2097152,262144,524288,1048576]
[ro.wifi.channels]: []
[wifi.interface]: [wlan0]
root@{yourboard}:/ # getprop | grep wlan
[dhcp.wlan0.dns1]: [192.168.1.1]
[dhcp.wlan0.dns2]: []
[dhcp.wlan0.dns3]: []
[dhcp.wlan0.dns4]: []
[dhcp.wlan0.domain]: []
[dhcp.wlan0.gateway]: [192.168.1.1]
[dhcp.wlan0.ipaddress]: [192.168.1.118]
[dhcp.wlan0.leasetime]: [86400]
[dhcp.wlan0.mask]: [255.255.255.0]
[dhcp.wlan0.pid]: [2689]
[dhcp.wlan0.reason]: [REBOOT]
[dhcp.wlan0.result]: [ok]
[dhcp.wlan0.server]: [192.168.1.1]
[dhcp.wlan0.vendorInfo]: []
[init.svc.dhcpcd_wlan0]: [running]
[wifi.interface]: [wlan0]
[wlan.driver.status]: [ok]
[wlan.interface]: [wlan0]
root@{yourboard}:/ # getprop | grep suppl
[init.svc.rtw_suppl]: [running]
root@{yourboard}:/ # cat /sys/kernel/debug/usb/devices
T: Bus=02 Lev=01 Prnt=01 Port=00 Cnt=01 Dev#= 2 Spd=480 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS=64 #Cfgs= 1
P: Vendor=0bda ProdID=8176 Rev= 2.00
S: Manufacturer=Realtek
S: Product=802.11n WLAN Adapter
S: SerialNumber=00e04c000001
C:* #Ifs= 1 Cfg#= 1 Atr=a0 MxPwr=500mA
I:* If#= 0 Alt= 0 #EPs= 4 Cls=ff(vend.) Sub=ff Prot=ff Driver=rtl8192cu
E: Ad=81(I) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=02(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=03(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=84(I) Atr=03(Int.) MxPS= 64 Ivl=125us
root@{yourboard}:/ # cat /sys/bus/usb/devices/2-1/product
802.11n WLAN Adapter
Useful commands:
disable wifi:
root@{yourboard}:/ # svc wifi disable
enable wifi:
root@{yourboard}:/ # svc wifi enable
open wifi settings panel:
root@{yourboard}:/ # am start -a android.intent.action.MAIN -n com.android.settings/.wifi.WifiSettings
manually starting supplicant with debug:
root@{yourboard}:/ # wpa_supplicant -Dnl80211 -iwlan0 -c/data/misc/wifi/wpa_supplicant.conf -dd -B
root@{yourboard}:/ # netcfg wlan0 up/down/dhcp
root@{yourboard}:/ # wpa_cli
> status
bssid=20:aa:4b:1b:a1:7c
ssid=ECTEST
id=0
mode=station
pairwise_cipher=NONE
group_cipher=NONE
key_mgmt=NONE
wpa_state=COMPLETED
ip_address=192.168.1.118
p2p_device_address=44:34:4c:8b:f2:10
address=44:34:4c:8b:f2:10
<3>CTRL-EVENT-STATE-CHANGE id=0 state=9 BSSID=20:aa:4b:1b:a1:7c SSID=ECTEST
<3>CTRL-EVENT-CONNECTED - connection to 20:aa:4b:1b:a1:7c completed (reauth) [id=0 id_str=]
> scan
cfg80211_rtw_scan(wlan0)
OK
> no packet in tx packet buffer (0)
survey done event(14) band:0 for wlan0
<3>CTRL-EVENT-SCAN-RESULTS
> scan_results
bssid / frequency / signal level / flags / ssid
20:aa:1b:1b:a1:7c 2437 -74 [WPS][ESS] ECTEST
00:1d:3e:bd:10:05 2457 -85 [WPA-PSK-TKIP][ESS] net02
68:7f:74:03:c6:be 2432 -59 [ESS] \x00\x00\x00\x00
c8:23:73:3f:05:71 2462 -66 [ESS] Nick's router. Hands off.
root@{yourboard}:/ # ifconfig wlan0
wlan0: ip 192.168.1.118 mask 255.255.255.0 flags [up broadcast running multicast]
root@{yourboard}:/ # dhcpcd wlan0
dhcpcd[3373]: version 5.5.6 starting
dhcpcd[3373]: wlan0: rebinding lease of 192.168.1.118
dhcpcd[3373]: wlan0: acknowledged 192.168.1.118 from 192.168.1.1
dhcpcd[3373]: wlan0: leased 192.168.1.118 for 86400 seconds
dhcpcd[3373]: forked to background, child pid 3405
root@{yourboard}:/ # netcfg
lo UP 127.0.0.1/8 0x00000049 00:00:00:00:00:00
eth0 UP 192.168.0.152/24 0x00001043 24:80:00:00:00:00
tunl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
sit0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
ip6tnl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
wlan0 UP 192.168.1.118/24 0x00001043 44:34:4c:8b:f2:10
wlan1 DOWN 0.0.0.0/0 0x00001002 46:34:4c:8b:f2:10
Good luck with it and please let me know if you need more info.
problem/solution:
if you get this problem:
E/wpa_supplicant( 3159): Could not set interface wlan0 flags (UP): Unknown error 132
solution:
missing rfkill, error 132 means "operation not possible due to RFkill"
vim kernel_imx/arch/arm/mach-mx6/board-mx6sl_{yourboard}.c
static int mx6sl_shd_bt_power_change(int status){return 0;}
static struct platform_device mxc_bt_rfkill = {
.name = "mxc_bt_rfkill",
};
static struct imx_bt_rfkill_platform_data mxc_bt_rfkill_data = {
.power_change = mx6sl_shd_bt_power_change,
};
/* init function */
static void __init {yourboard}_init(void){
...
mxc_register_device(&mxc_bt_rfkill, &mxc_bt_rfkill_data);
}
problem:
E/WifiHW ( 2488): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": No such file or directory
solution:
setup correctly in init.rc and init.freescale.rc scripts wifi and wpa_supplicant permissions and services.
Hi,
I am trying to bring up wifi in i.mx6 sabreauto6q board using Netgear usb dongle. Can any one please help me with Boardconfig.mk file for adding support for ath9k?
This is my configuration:
#BOARD_WLAN_DEVICE | := UNITE |
#WPA_SUPPLICANT_VERSION | := VER_0_8_UNITE |
TARGET_KERNEL_MODULES | := \ |
kernel_imx/drivers/net/wireless/rtl8723as/8723as.ko:system/lib/modules/8723as.ko \ | |
kernel_imx/net/wireless/cfg80211.ko:system/lib/modules/cfg80211_realtek.ko |
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
BOARD_HOSTAPD_DRIVER | := NL80211 |
BOARD_HOSTAPD_PRIVATE_LIB_QCOM | := lib_driver_cmd_qcwcn |
BOARD_WPA_SUPPLICANT_PRIVATE_LIB_QCOM | := lib_driver_cmd_qcwcn |
BOARD_HOSTAPD_PRIVATE_LIB_RTL | := lib_driver_cmd_rtl |
BOARD_WPA_SUPPLICANT_PRIVATE_LIB_RTL | := lib_driver_cmd_rtl |
# Wifi
BOARD_WLAN_VENDOR | := ATHEROS |
# for atheros vendor
ifeq ($(BOARD_WLAN_VENDOR),ATHEROS)
BOARD_WLAN_DEVICE | := ar9485 |
BOARD_HAS_ATH_WLAN | := true |
WPA_SUPPLICANT_VERSION | := VER_0_8_ATHEROS |
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
#BOARD_HOSTAPD_PRIVATE_LIB | := lib_driver_cmd |
#BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd
WIFI_DRIVER_MODULE_PATH := "/system/lib/modules/ath9k_htc.ko"
WIFI_DRIVER_MODULE_NAME := "ath9k_htc"
WIFI_SDIO_IF_DRIVER_MODULE_PATH := "/system/lib/modules/cfg80211.ko"
WIFI_SDIO_IF_DRIVER_MODULE_NAME := "cfg80211"
WIFI_SDIO_IF_DRIVER_MODULE_ARG := ""
WIFI_COMPAT_MODULE_PATH := "/system/lib/modules/compat.ko"
WIFI_COMPAT_MODULE_NAME := "compat"
WIFI_COMPAT_MODULE_ARG | := "" |
endif
As mentioned in this thread , am able to connect to wifi from terminal. Please give some suggestions.
Thanks and regards,
Arun S
Hi All,
I am working to bring up RealTek USB wifi (rtl8188cu) dongel on android 4.3 and kernel 3.0.35 below are steps I followed :
Step 1) I am building rtl8192cu as module. I made the other components MAC80211 and CFG80211 as built in.
root@nitrogen6x:/ # cat /sys/kernel/debug/usb/devices
...
T: Bus=02 Lev=02 Prnt=02 Port=00 Cnt=01 Dev#= 3 Spd=480 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS=64 #Cfgs= 1
P: Vendor=0bda ProdID=8176 Rev= 2.00
S: Manufacturer=Realtek
S: Product=802.11n WLAN Adapter
S: SerialNumber=00e04c000001
C:* #Ifs= 1 Cfg#= 1 Atr=a0 MxPwr=500mA
I:* If#= 0 Alt= 0 #EPs= 4 Cls=ff(vend.) Sub=ff Prot=ff Driver=rtl8192cu
E: Ad=81(I) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=02(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=03(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=84(I) Atr=03(Int.) MxPS= 64 Ivl=125us
...
root@nitrogen6x:/ # dmesg
rtl8192cu driver version=v4.0.2_9000.20130911
build time: Feb 2 2015 14:05:08
usb_endpoint_descriptor(0):
bLength=7
bDescriptorType=5
bEndpointAddress=81
wMaxPacketSize=200
bInterval=0
RT_usb_endpoint_is_bulk_in = 1
usb_endpoint_descriptor(1):
bLength=7
bDescriptorType=5
bEndpointAddress=2
wMaxPacketSize=200
bInterval=0
RT_usb_endpoint_is_bulk_out = 2
usb_endpoint_descriptor(2):
bLength=7
bDescriptorType=5
bEndpointAddress=3
wMaxPacketSize=200
bInterval=0
RT_usb_endpoint_is_bulk_out = 3
usb_endpoint_descriptor(3):
bLength=7
bDescriptorType=5
bEndpointAddress=84
wMaxPacketSize=40
bInterval=1
RT_usb_endpoint_is_int_in = 4, Interval = 1
nr_endpoint=4, in_num=2, out_num=2
USB_SPEED_HIGH
CHIP TYPE: RTL8188C_8192C
register rtw_netdev_ops to netdev_ops
Chip Version ID: VERSION_NORMAL_UMC_CHIP_88C_B_CUT.
RF_Type is 3!!
EEPROM type is E-FUSE
====> ReadAdapterInfo8192C
Boot from EFUSE, Autoload OK !
EEPROMVID = 0x0bda
EEPROMPID = 0x8176
EEPROMCustomerID : 0x00
EEPROMSubCustomerID: 0x00
RT_CustomerID: 0x00
_ReadMACAddress MAC Address from EFUSE = 44:33:4c:80:cb:1e
EEPROMRegulatory = 0x0
_ReadBoardType(0)
BT Coexistance = disable
mlmepriv.ChannelPlan = 0x08
_ReadPSSetting...bHWPwrPindetect(0)-bHWPowerdown(10) ,bSupportRemoteWakeup(0)
### PS params=> power_mgnt(1),usbss_enable(0) ###
### AntDivCfg(0)
readAdapterInfo_8192CU(): REPLACEMENT = 0
<==== ReadAdapterInfo8192C in 240 ms
rtw_register_early_suspend
rtw_macaddr_cfg MAC Address = 44:33:4c:80:cb:1e
bDriverStopped:1, bSurpriseRemoved:0, bup:0, hw_init_completed:0
_rtw_drv_register_netdev, MAC Address (if1) = 44:33:4c:80:cb:1e
usbcore: registered new interface driver rtl8192cu
init: no such service ''
mtp_open
init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
Step 2) wlan0 interface is creating successfully in /sys/class/net/wlan0.
root@nitrogen6x:/ # ls -l /sys/class/net/wlan0
lrwxrwxrwx root root 2004-06-05 17:54 wlan0 -> ../../devices/platform/fsl-ehci.1/usb2/2-1/2-1.1/2-1.1:1.0/net/wlan0
root@nitrogen6x:/ # ls -l /sys/devices/platform/fsl-ehci.1/usb2/2-1/2-1.1/2-1.1:1.0/net/wlan0
-r--r--r-- root root 4096 2004-06-05 17:54 addr_assign_type
-r--r--r-- root root 4096 2004-06-05 17:54 addr_len
-r--r--r-- root root 4096 2004-06-05 17:54 address
-r--r--r-- root root 4096 2004-06-05 17:54 broadcast
-r--r--r-- root root 4096 2004-06-05 17:54 carrier
-r--r--r-- root root 4096 2004-06-05 17:54 dev_id
lrwxrwxrwx root root 2004-06-05 17:54 device -> ../../../2-1.1:1.0
-r--r--r-- root root 4096 2004-06-05 17:54 dormant
-r--r--r-- root root 4096 2004-06-05 17:54 duplex
-r--r--r-- root root 4096 2004-06-05 17:54 features
-rw-r--r-- root root 4096 2004-06-05 17:54 flags
-rw-r--r-- root root 4096 2004-06-05 17:54 ifalias
-r--r--r-- root root 4096 2004-06-05 17:54 ifindex
-r--r--r-- root root 4096 2004-06-05 17:54 iflink
-r--r--r-- root root 4096 2004-06-05 17:54 link_mode
-rw-r--r-- root root 4096 2004-06-05 17:54 mtu
-rw-r--r-- root root 4096 2004-06-05 17:54 netdev_group
-r--r--r-- root root 4096 2004-06-05 17:54 operstate
drwxr-xr-x root root 2004-06-05 17:54 power
drwxr-xr-x root root 2004-06-05 17:54 queues
-r--r--r-- root root 4096 2004-06-05 17:54 speed
drwxr-xr-x root root 2004-06-05 17:54 statistics
lrwxrwxrwx root root 2004-06-05 17:54 subsystem -> ../../../../../../../../../class/net
-rw-r--r-- root root 4096 2004-06-05 17:54 tx_queue_len
-r--r--r-- root root 4096 2004-06-05 17:54 type
-rw-r--r-- root root 4096 2004-06-05 17:54 uevent
drwxr-xr-x root root 2004-06-05 17:54 wireless
Step 3) After that I try to run below command.
root@nitrogen6x:/ # dhcpcd wlan0
dhcpcd[3264]: version 5.5.6 start+871x_drv - drv_open, bup=0
ing
===> FirmwareDownload91C() fw:Rtl819XFwImageArray_UMC_B
FirmwareDownload92C accquire FW from embedded image
fw_ver=v88, fw_subver=2, sig=0x88c0
fw download ok!
Set RF Chip ID to RF_6052 and RF type to 1T1R.
IQK:Start!!!
Path A IQK Success!!
Path A IQK Success!!
IQK: final_candidate is 0
IQK: RegE94=102 RegE9C=10 RegEA4=fa RegEAC=3 RegEB4=0 RegEBC=0 RegEC4=0 RegECC=0
Path A IQ Calibration Success !
pdmpriv->TxPowerTrackControl = 1
rtl8192cu_hal_init in 610ms
MAC Address = 44:33:4c:80:cb:1e
-871x_drv - drv_open, bup=1
ADDRCONF(NETDEV_UP): wlan0: link is not ready
dhcpcd[3264]: wlan0: sending IPv6 Router Solicitation
dhcpcd[3264]: wlan0: sendmsg: Network is unreachable
dhcpcd[3264]: wlan0: checking for 169.254.156.2
==>rtw_ps_processor .fw_state(0)
==>ips_enter cnts:1
===> rtw_ips_pwr_down...................
====> rtw_ips_dev_unload...
usb_read_port_cancel
usb_read_port_complete()-1284: RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0) bReadPortCancel(1)
usb_read_port_complete()-1284: RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0) bReadPortCancel(1)
usb_read_port_complete()-1284: RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0) bReadPortCancel(1)
usb_read_port_complete()-1284: RX Warning! bDriverStopped(0) OR bSurpriseRemoved(0) bReadPortCancel(1)
usb_write_port_cancel
==> rtl8192cu_hal_deinit
bkeepfwalive(0)
card disble without HWSM...........
<=== rtw_ips_pwr_down..................... in 90ms
dhcpcd[3264]: wlan0: sending IPv6 Router Solicitation
dhcpcd[3264]: wlan0: sendmsg: Network is unreachable
dhcpcd[3264]: wlan0: using IPv4LL address 169.254.156.2
dhcpcd[3264]: forked to background, child pid 3291
Step 4) If I turn on wifi from Android settings, I only see the following message from logcat:
D/WifiService( 2746): setWifiEnabled: true pid=2997, uid=1000
kindly help me to solve issue.
Thanks In Advance,
Sami Iqneibi
Hello Sami,
Next is for WifiService to Invoking mWifiStateMachine.setWifiEnabled.
This could be something simple, like permissions. Could you check that?
If you run some wifi setup programs, like dhcpcd or wpa_supplicant, you should restart the system, just to be sure. Android's wifi is very sensitive :-).
Also, you could include more debug:
frameworks/base/wifi/java/android/net/wifi/*.java
frameworks/base/services/java/com/android/server/wifi/*.java
private static final boolean DBG = true;
When you turn wifi on from Android settings, it will run wpa_supplicant service, so if you added debug argument (-dd) you should see more in logcat..
BR,
Zoran
Hi Zoran,
Thank you for your help.
I noticed that when I run wpa_supplicant from the command shell as follows:
wpa_supplicant -Dnl80211 -iwlan0 -c/data/misc/wifi/wpa_supplicant.conf -dd -B
I get the error:
D/wpa_supplicant( 3901): Could not open file /sys/class/net/wlan0/phy80211/name: No such file or directory
So, I checked the contents of /sys/class/net/wlan0 and found that phy80211 is missing.
I checked my kernel settings in .config file to find that I have these set as follows:
CONFIG_CFG80211=y
CONFIG_NL80211_TESTMODE=y
CONFIG_CFG80211_DEFAULT_PS=y
CONFIG_CFG80211_WEXT=y
CONFIG_MAC80211=y
CONFIG_HOSTAP=y
CONFIG_RTL8192CU=m
and found that those are missing
# CONFIG_USB_USBNET is not set
# CONFIG_NET_RADIO is not set
It seems that I am not building the realtek driver for nl80211 protocol.
I got some compilation errors when I tried to change those settings. I will try some more and come back with results later.
I really appreciate your help with this matter.
Best regards,
Sami
Hi Sami:
I am facing the same troble with your met about the wifi ap mode. when i use the commad "hostapd -d /etc/hostapd.conf" :
could not open file /sys/class/net/wlan0/phy80211/name: No such file or directory
can you share your experience,and give me some advise?
thank you in advance!
Hi Neal,
The real authority on this subject is Zoran but I will try my best to answer your question (and Zoran can correct me if I am wrong).
There are two Linux wireless API: WEXT, CFG80211.
In order to enable the CFG80211 API, you need to define CONFIG_IOCTL_CFG80211.
I fixed my problem "could not open file /sys/class/net/wlan0/phy80211/name" by changing the following compile switches in
kernel_imx/drivers/net/wireless/rtl8192cu/include/autoconf.h:
#define CONFIG_IOCTL_CFG80211 1
#ifdef CONFIG_IOCTL_CFG80211
#define RTW_USE_CFG80211_STA_EVENT /* Indecate new sta asoc through cfg80211_new_sta */
//#define CONFIG_CFG80211_FORCE_COMPATIBLE_2_6_37_UNDER
#define CONFIG_DEBUG_CFG80211 1
Best regards,
Sami
Hi Sami,
You can try to build driver as integrated =y, maybe you'll get more info during build.
Do you insert all the modules needed, in the right order?
Do you have this in your BoardConfig,mk file:
CONFIG_DRIVER_NL80211 := true
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_rtl
NL80211 supposed to replace WEXT, so maybe disabling the WEXT to build could give you more info.
I also have:
# CONFIG_USB_USBNET is not set
# CONFIG_NET_RADIO is not setvv
NP. Let me know is you need more help
BR,
Zoran
Also, for wifi to work on android dont forget to add system/netd/SoftapController_realtek.cpp and modify system/netd/SoftapController.h.
vim system/netd/SoftapController.h
#ifndef _SOFTAP_CONTROLLER_H
#define _SOFTAP_CONTROLLER_H
#include <linux/in.h>
#include <net/if.h>
#include <utils/List.h>
#define SOFTAP_MAX_BUFFER_SIZE 4096
#define AP_BSS_START_DELAY 200000
#define AP_BSS_STOP_DELAY 500000
#define AP_SET_CFG_DELAY 500000
#define AP_DRIVER_START_DELAY 800000
class SoftapController {
int mSock;
int addParam(int pos, const char *cmd, const char *arg);
int setCommand(char *iface, const char *fname, unsigned buflen=0);
char mIface[IFNAMSIZ];
char mBuf[SOFTAP_MAX_BUFFER_SIZE];
public:
SoftapController();
virtual ~SoftapController();
int startSoftap();
int stopSoftap();
bool isSoftapStarted();
int setSoftap(int argc, char *argv[]);
int fwReloadSoftap(int argc, char *argv[]);
int startDriver(char *iface) ;
int stopDriver(char *iface) ;
int clientsSoftap(char **retbuf);
Hi Zoran,
Thank you for your continuous help.
Where do I get the "SoftapController_realtek.cpp" from? and Do I really need it if I don't want my wifi dongle to work as SoftAP?
I have made some progress in the last week.
I was able to build the realtek driver after changing a couple of compile switches and get the NL80211 protocol working.
The realtek wifi dongle is now working if I start it up manually.
What I mean by starting it manually is:
- If I start my board while the wifi dongle is inserted into the USB connector. The wifi dongle will not work. I have to disconnect it and then connect it back.
- After the wifi dongle works, I need to start the dhcpcd from the console
root@nitrogen6x:/ # dhcpcd wlan0
- After the wifi dongle takes an IP address, I can start the wpa_supplicant as a service:
root@nitrogen6x:/ # start rtw_suppl
- Then I can start the wpa_cli, scan for networks, connect to one network, and ping the internet.
My current problems are:
- Realtek dongle will not automatically start
- dhcpcd_wlan0 service doesnot start automatically and will not start manually (i.e. with "start dhcpcd_wlan0" command from console)
- When I try to enable wifi from Android UI setting, nothing happens.
I saw your message in this thread to Ranganath tm to send the following files/folders:
out/target/product/{yourdevice}/system/etc/wifi/wpa_supplicant.conf
out/target/product/{yourdevice}/root//init.rc
out/target/product/{yourdevice}/root/init.{yourdevice}.rc
out/target/product/{yourboard}/system/etc/permissions
hardware/realtek
hardware/libhardware_legacy
external/wpa_supplicant_8
kernel_imx/arch/arm/configs/imx6s_{yourdevice}_android_defconfig
device/fsl/{yourdevice}/BoardConfig.mk
frameworks/base/wifi/java/android/net/wifi
Please list all relevant folders/files to recheck permissions!
Could you send those files/folders to me or I could send you mine (if you prefer)?
I have already sent you my email in a PM (I hope you don't mind).
Best regards,
Sami
Hi Zoran,
Thank you very much for your help.
I made all the changes you suggested in your private message and the realtek wifi adaptor is finally working properly.
My last permissions problem was:
03-05 14:22:16.460: E/WifiHW(2779): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": No such file or directory
It was fixed when I deleted the folder:
/data/system/wpa_supplicant
as suggested by the link you gave me in your last email:
http://blog.linuxconsulting.ro/2010/04/porting-wifi-drivers-to-android.html
Thanks again.
best regards,
Sami
Hello Sami,
Great to hear that, you are very welcome.
BR,
Zoran
Hi, Zoran
what Android was used, is it Freescale Android (link below) ?
IMX6_JB43_110_ANDROID_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo and i.MX 6Sololite Android jb4.3_1.1.0 0 BSP, Documentation and Source Code
Also very often WiFi modules have different firmware, so different drivers are needed, though module
name may the same. Have you contacted Realtek for updated version of driver for this specific module ?
Hello,
Thank you for answering,
Yeah, I wanted to add that info. It was JB4.3 and the Realtek porting for rtl8192cu driver is for JB4.2.
Some more porting work was needed to be done that wasnt in the manual.
Also we are currently working on nfs, there shouldnt be some permissions problem.
We put every all firmware files in the root fs (nfs) just in case.
ls /system/etc/firmware/rtlwifi/ -l
-rw------- root root 11216 2014-04-23 13:10 rtl8188efw.bin
-rw------- root root 13904 2014-04-23 13:10 rtl8188eufw.bin
-rw------- root root 13540 2014-04-23 13:10 rtl8192cfw.bin
-rw------- root root 14818 2014-04-23 13:10 rtl8192cfwU.bin
-rw------- root root 14800 2014-04-23 13:10 rtl8192cfwU_B.bin
-rw------- root root 16014 2014-04-23 13:10 rtl8192cufw.bin
-rw------- root root 16116 2014-04-23 13:10 rtl8192cufw_A.bin
-rw------- root root 16096 2014-04-23 13:10 rtl8192cufw_B.bin
-rw------- root root 16116 2014-04-23 13:10 rtl8192cufw_TMSC.bin
-rw------- root root 22978 2014-04-23 13:10 rtl8192defw.bin
-rw------- root root 32754 2014-04-23 13:10 rtl8192eefw.bin
-rw------- root root 80208 2014-04-23 13:10 rtl8192sefw.bin
-rw------- root root 122328 2014-04-23 13:10 rtl8712u.bin
-rw------- root root 22172 2014-04-23 13:10 rtl8723aufw_A.bin
-rw------- root root 24118 2014-04-23 13:10 rtl8723aufw_B.bin
-rw------- root root 19200 2014-04-23 13:10 rtl8723aufw_B_NoBT.bin
-rw------- root root 11662 2014-04-23 13:10 rtl8723fw.bin
-rw------- root root 22996 2014-04-23 13:10 rtl8723fw_B.bin
-rw------- root root 29198 2014-04-23 13:10 rtl8821aefw.bin
but driver source it askes for:
(kernel_imx/drivers/net/wireless/rtlwifi/rtl8192cu/sw.c file)
MODULE_FIRMWARE("rtlwifi/rtl8192cufw.bin");
also, driver is build in the kernel, from boot:
rtl8192cu driver version=v4.0.2_9000.20130911
build time: Apr 24 2014 13:14:21
usbcore: registered new interface driver rtl8192cu
..
USB_SPEED_HIGH
CHIP TYPE: RTL8188C_8192C
register rtw_netdev_ops to netdev_ops
android_work: sent uevent USB_STATE=CONNECTED
Netfilter messages via NETLINK v0.30.
android_work: sent uevent USB_STATE=DISCONNECTED
Chip Version ID: VERSION_NORMAL_UMC_CHIP_88C_B_CUT.
nf_conntrack version 0.5.0 (7141 buckets, 28564 max)
RF_Type is 3!!
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
...
readAdapterInfo_8192CU(): REPLACEMENT = 0
<==== ReadAdapterInfo8192C in 570 ms
rtw_register_early_suspend
rtw_macaddr_cfg MAC Address = 44:33:4c:8b:f2:10
bDriverStopped:1, bSurpriseRemoved:0, bup:0, hw_init_completed:0
This shouldn't be a problem:
-rw------- root root
because system handles driver. But I will check out this, more.
Other thing is that wpa_supplicant isnt not called from init script, there is no trace of it in logcat.
in init.freescale.rs file:
service wpa_supplicant /system/bin/wpa_supplicant -iwlan0 -Dnl80211 \
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class late_start
disabled
oneshot
service p2p_supplicant /system/bin/wpa_supplicant \
-ip2p0 -Dnl80211 -c/data/misc/wifi/p2p_supplicant.conf -N \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf
class late_start
disabled
oneshot
service rtw_suppl_con /system/bin/rtl_wpa_supplicant \
-ip2p0 -Dnl80211 -c/data/misc/wifi/p2p_supplicant.conf -e/data/misc/wifi/entropy.bin -N \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf
class late_start
socket wpa_wlan0 dgram 660 wifi wifi
disabled
oneshot
service rtw_suppl /system/bin/wpa_supplicant -iwlan0 -Dnl80211a \
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class main
disabled
oneshot
service dhcpcd_wlan0 /system/bin/dhcpcd -aABKL
class main
disabled
oneshot
service dhcpcd_p2p /system/bin/dhcpcd -aABKL
class main
disabled
oneshot
service iprenew_wlan0 /system/bin/dhcpcd -n
class main
disabled
oneshot
service iprenew_p2p /system/bin/dhcpcd -n
class main
disabled
oneshot
in init.rs file:
# give system access to wpa_supplicant.conf for backup and restore
mkdir /data/misc/wifi 0770 wifi wifi
chmod 0770 /data/misc/wifi
mkdir /data/misc/wifi/sockets 0770 wifi wifi
mkdir /data/misc/wifi/wpa_supplicant 0770 wifi wifi
mkdir /data/misc/wifi/p2p_supplicant 0770 wifi wifi
mkdir /data/misc/dhcp 0770 dhcp dhcp
chown dhcp dhcp /data/misc/dhcp
chmod 0660 /data/misc/wifi/wpa_supplicant.conf
chmod 0660 /data/misc/wifi/p2p_supplicant.conf
chmod 0775 /system/etc/dhcpcd/dhcpcd-run-hooks
######for nfs maybe some permissions problems (didn't work)
# chown system wifi /data/misc/wifi
# chown system wifi /data/misc/wifi/wpa_supplicant.conf
# chown system wifi /system/etc/wifi/wpa_supplicant.conf
If we manual start dhcp for wlan0, we can get wifi ip address (in my previous post).
When we manually call wpa_supplicant:
wpa_supplicant -iwlan0 -c/system/etc/wifi/wpa_supplicant.conf -B
we get this in logcat:
--------- beginning of /dev/log/main
I/wpa_supplicant( 2938): Successfully initialized wpa_supplicant
E/wpa_supplicant( 2938): nl80211: Could not add multicast membership for scan events: -2 (No such file or directory)
E/wpa_supplicant( 2938): Failed to initialize driver 'nl80211'
In board config file:
(./device/fsl/evk_6sl/BoardConfig.mk file)
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
BOARD_HOSTAPD_DRIVER := NL80211
in both
./external/wpa_supplicant_8/wpa_supplicant/android.config
and
./external/wpa_supplicant_8/hostapd/android.config
CONFIG_DRIVER_NL80211=y
We didn't contacted Realtek yet, we believe that we have some binding problems with driver and android ui.
Also, slider button for wifi in the Settings menu in the Android ui seamed not to be connected to Settings>Wifi button.
I can move button in Settings menu, to On state. And the enter the Settings>Wi-Fi and the button is in Off state.
Exiting Settings>Wi-Fi menu and entering it again, it shows that button is back in Off state.
Toggling wifi button to Off state isn't possible, after it was set to On state by us.
After moving the wifi button slider to Off state we get this in logcat:
D/WifiService( 2401): setWifiEnabled: true pid=2561, uid=1000
E/WifiService( 2401): Invoking mWifiStateMachine.setWifiEnabled
in system/core/include/private/android_filesystem_config.h file we can see uid's
#define AID_SYSTEM 1000 /* system server */
#define AID_WIFI 1010 /* wifi subsystem */
Do we need to register platform driver callbacks, but this is usb module, it shouldn't need that?
Is it some nfs permission related issue with wifi?
So, what do you think?
building the driver as module also doesn't work ..
we are pretty sure that it is to android binding with driver.
we tried three different drivers for rtl8192cu.
root@evk_6sl:/ # insmod /system/lib/modules/cfg80211_realtek.ko
cfg80211: Calling CRDA to update world regulatory domain
root@evk_6sl:/ # insmod /system/lib/modules/8192cu.ko
rtl8192cu driver version=v4.0.2_9000.20130911
build time: Apr 25 2014 15:18:54
usb_endpoint_descriptor(0):
bLength=7
bDescriptorType=5
bEndpointAddress=81
wMaxPacketSize=200
bInterval=0
RT_usb_endpoint_is_bulk_in = 1
usb_endpoint_descriptor(1):
bLength=7
bDescriptorType=5
bEndpointAddress=2
wMaxPacketSize=200
bInterval=0
RT_usb_endpoint_is_bulk_out = 2
usb_endpoint_descriptor(2):
bLength=7
bDescriptorType=5
bEndpointAddress=3
wMaxPacketSize=200
bInterval=0
RT_usb_endpoint_is_bulk_out = 3
usb_endpoint_descriptor(3):
bLength=7
bDescriptorType=5
bEndpointAddress=84
wMaxPacketSize=40
bInterval=1
RT_usb_endpoint_is_int_in = 4, Interval = 1
nr_endpoint=4, in_num=2, out_num=2
USB_SPEED_HIGH
CHIP TYPE: RTL8188C_8192C
register rtw_netdev_ops to netdev_ops
Chip Version ID: VERSION_NORMAL_UMC_CHIP_88C_B_CUT.
RF_Type is 3!!
EEPROM type is E-FUSE
====> ReadAdapterInfo8192C
Boot from EFUSE, Autoload OK !
EEPROMVID = 0x0bda
EEPROMPID = 0x8176
EEPROMCustomerID : 0x00
EEPROMSubCustomerID: 0x00
RT_CustomerID: 0x00
_ReadMACAddress MAC Address from EFUSE = 44:33:4c:8b:f2:10
EEPROMRegulatory = 0x0
_ReadBoardType(0)
BT Coexistance = disable
mlmepriv.ChannelPlan = 0x08
_ReadPSSetting...bHWPwrPindetect(0)-bHWPowerdown(10) ,bSupportRemoteWakeup(0)
### PS params=> power_mgnt(0),usbss_enable(0) ###
### AntDivCfg(0)
readAdapterInfo_8192CU(): REPLACEMENT = 0
<==== ReadAdapterInfo8192C in 180 ms
rtw_wdev_alloc(padapter=da5f7000)
rtw_register_early_suspend
rtw_macaddr_cfg MAC Address = 44:33:4c:8b:f2:10
bDriverStopped:1, bSurpriseRemoved:0, bup:0, hw_init_completed:0
register rtw_netdev_ops to netdev_ops
register rtw_netdev_if2_ops to netdev_ops
rtw_wdev_alloc(padapter=db8e7000)
Chip Version ID: VERSION_NORMAL_UMC_CHIP_88C_B_CUT.
RF_Type is 3!!
_rtw_drv_register_netdev, MAC Address (if1) = 44:33:4c:8b:f2:10
_rtw_drv_register_netdev, MAC Address (if2) = 46:33:4c:8b:f2:10
usbcore: registered new interface driver rtl8192cu
here is this kernel build config file:
CONFIG_WLAN=y
CONFIG_WIFI_CONTROL_FUNC=y
CONFIG_HOSTAP=y
CONFIG_CFG80211=m
CONFIG_NL80211_TESTMODE=y
CONFIG_CFG80211_REG_DEBUG=y
CONFIG_CFG80211_DEFAULT_PS=y
CONFIG_CFG80211_DEBUGFS=y
CONFIG_CFG80211_WEXT=y
CONFIG_LIB80211=y
CONFIG_LIB80211_CRYPT_WEP=y
CONFIG_LIB80211_CRYPT_CCMP=y
CONFIG_LIB80211_CRYPT_TKIP=y
CONFIG_CFG80211_ALLOW_RECONNECT=y
CONFIG_MAC80211=m
CONFIG_MAC80211_HAS_RC=y
CONFIG_MAC80211_RC_MINSTREL=y
CONFIG_MAC80211_RC_MINSTREL_HT=y
CONFIG_MAC80211_RC_DEFAULT_MINSTREL=y
CONFIG_MAC80211_RC_DEFAULT="minstrel_ht"
CONFIG_MAC80211_MESH=y
CONFIG_RTL8192CU=m
root@evk_6sl:/ # lsmod
8192cu 674910 0 - Live 0x00000000
cfg80211 155527 1 8192cu, Live 0x00000000
before that driver was build as part of kernel:
CONFIG_RTL8192CU=y
Hi Zoran, I got advice from our expert:
I had been reading about this issue and also i read the description from the client and seem
there's some missing configuration which the client could try.
First of all try to set BOARD_WPA_SUPPLICANT_DRIVER to WEXT in the Android BSP.
Also you need to provide a proper wpa configuration file for your device.
For more details check this reference:
PaNiC Random Rant (or how we used to call it: .plan): Porting WiFi drivers to Android
Hope this helps
Yep, I tried this link.
In manual provided with rtl wifi driver, it states to use new nl80211 interface.
BoardConfig.mk
BOARD_WPA_SUPPLICANT_DRIVER=NL80211
Problem is that Wifi slider switch cant be moved, but nothing happens, so some binding or some permissions are problem. This is done in nfs.
When slider is moved to On position in logcat we get this:
D/WifiService( 2401): setWifiEnabled: true pid=2561, uid=1000
E/WifiService( 2401): Invoking mWifiStateMachine.setWifiEnabled
there should be more data or some error or permission staff for wifi, after this.
wpa_supplicant doesnt start automatically, but it is in init.freescale.rc script. It can start manually with nl80211 driver.
WEXT, I will try this again, thank you. I am not sure it will work, i dont think the driver is problem. I can scan and get all networks in area, using shell.
We have a similar setup and are having the same problems. Right down to the same bogus IP address reported by netconfig after dhcpcd seems to believe it got an address from the DHCP server on my Access Point.
Has there been any activity on this?
Yes, we manage to get wifi working. Here are info's in more detail, so if anybody else has problem ...
We build driver as part of the kernel:
vim kernel_imx/arch/arm/configs/imx6s_{yourdevice}_android_defconfig
CONFIG_CFG80211=y
CONFIG_MAC80211_MESH=y
CONFIG_MAC80211=y
CONFIG_HOSTAP=y
CONFIG_RTL8192CU=y
CONFIG_RTLWIFI=y
CONFIG_RTL8192C_COMMON=y
#CONFIG_RTL8723AS=m
CONFIG_USB_USBNET=y
CONFIG_NET_RADIO=y
vim device/fsl/{yourdevice}/BoardConfig.mk
BOARD_WIFI_VENDOR := realtek
WPA_SUPPLICANT_VERSION := VER_0_8_X
CONFIG_DRIVER_NL80211 := true
BOARD_WPA_SUPPLICANT_DRIVER := NL80211
BOARD_WPA_SUPPLICANT_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_HOSTAPD_DRIVER := NL80211
BOARD_HOSTAPD_PRIVATE_LIB := lib_driver_cmd_rtl
BOARD_WLAN_DEVICE := rtl8192cu
WIFI_DRIVER_MODULE_NAME := "wlan0"
WIFI_DRIVER_MODULE_PATH := ""
WIFI_DRIVER_MODULE_ARG := ""
WIFI_FIRMWARE_LOADER := ""
WIFI_DRIVER_FW_PATH_STA := ""
WIFI_DRIVER_FW_PATH_AP := ""
WIFI_DRIVER_FW_PATH_P2P := ""
WIFI_DRIVER_FW_PATH_PARAM := ""
We disabled p2p, since we dont need it:
vim device/fsl/imx6/{yourboard}.mk
PRODUCT_COPY_FILES += \
#frameworks/native/data/etc/android.hardware.wifi.direct.xml:system/etc/permissions/android.hardware.wifi.direct.xml
or
rm out/target/product/{yourboard}/system/etc/permissions/android.hardware.wifi.direct.xml
or just remount system partition:
root@{yourboard}:/ # mount -o remount, rw /system;
and remove xml:
root@{yourboard}:/ # rm /system/etc/permissions/android.hardware.wifi.direct.xml
edit:
root@{yourboard}:/ # busybox vi system/etc/permissions/required_hardware.xml
or
vim device/fsl/{yourboard}/required_hardware.xml
or
vim out/target/product/{yourboard}/system/etc/permissions/required_hardware.xml
<!--
<feature name="android.hardware.wifi.direct" />
-->
If you use it as module, you will need to add it also in PRODUCT_COPY_FILES
You need to correct init scripts, leave just this lines:
(this is from: http://blog.linuxconsulting.ro/2010/04/porting-wifi-drivers-to-android.html )
You can do it directly to out folder:
vim out/target/product/{yourboard}/root/init.rc
or/and (rebuild the whole system):
vim device/fsl/imx6/imx6.mk
mkdir /system/etc/wifi 0770 wifi wifi
chmod 0770 /system/etc/wifi
chmod 0660 /system/etc/wifi/wpa_supplicant.conf
chown wifi wifi /system/etc/wifi/wpa_supplicant.conf
#wpa_supplicant control socket for android wifi.c (android private socket)
mkdir /data/misc/wifi 0770 wifi wifi
mkdir /data/misc/wifi/sockets 0770 wifi wifi
chmod 0770 /data/misc/wifi
chmod 0660 /data/misc/wifi/wpa_supplicant.conf
chown wifi wifi /data/misc/wifi
chown wifi wifi /data/misc/wifi/wpa_supplicant.conf
setprop wifi.interface wlan0
setprop wlan.driver.status "ok"
#setprop wifi.ap.interface wlan0
#and also remove this lines:
# mkdir /data/system/wpa_supplicant 0771 wifi wifi
# chmod 0771 /data/system/wpa_supplicant
# symlink /data/misc/wifi/wpa_supplicant /data/system/wpa_supplicant
you can read it in that blog link, about unix/android standard socket setup.
vim out/target/product/{yourboard}/root/init.freescale.rc
or/and
vim device/fsl/{yourboard}/init.rc
#this is the only supplicant service and dhcpcd service for wifi that we use:
service rtw_suppl /system/bin/wpa_supplicant -dd -iwlan0 -Dnl80211 \
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class main
disabled
oneshot
service dhcpcd_wlan0 /system/bin/dhcpcd -aABKL
class main
disabled
oneshot
service iprenew_wlan0 /system/bin/dhcpcd -n
class main
disabled
oneshot
To keep it clean (it doesnt effect wifi):
vim device/fsl/imx6/imx6.mk
PRODUCT_PACKAGES += \
rtw_suppl \
We needed to make a little change in wifi_realtek.c since our jb is 4.3:
vim hardware/realtek/wlan/libhardware_legacy/wifi/wifi_realtek.c
int wifi_start_supplicant(int p2p_supported)
..
wifi_stop_supplicant(p2p_supported);
….
int wifi_stop_supplicant(int p2p_supported){
char supp_status[PROPERTY_VALUE_MAX] = {'\0'};
int count = 50; /* wait at most 5 seconds for completion */
if (p2p_supported) {
property_get("wifi.supplicant", supplicant_name, P2P_SUPPLICANT_NAME);
snprintf(supplicant_prop_name, PROPERTY_KEY_MAX, P2P_PROP_NAME, supplicant_name);
} else {
property_get("wifi.supplicant", supplicant_name, SUPPLICANT_NAME);
snprintf(supplicant_prop_name, PROPERTY_KEY_MAX, SUPP_PROP_NAME, supplicant_name);
}
Our problem was wrong supplicant name in prop setup. And, when wifi starts it first stops supplicant, and it wasn’t able to transfer that info through system. It was quite fun tracking this problem.
vim ./frameworks/base/wifi/java/android/net/wifi/WifiStateMachine.java
mWifiNative.killSupplicant(mP2pSupported);
if(mWifiNative.startSupplicant(mP2pSupported)) {
setWifiState(WIFI_STATE_ENABLING);
if (DBG) log("Supplicant start successful");
mWifiMonitor.startMonitoring();
transitionTo(mSupplicantStartingState);
} else {
loge("Failed to start supplicant!!");
}
Here are more info:
root@{yourdevice}:/ # cat /data/misc/wifi/wpa_supplicant.conf
ctrl_interface=wlan0
update_config=1
device_name={yourdevice}
manufacturer=Freescale
model_name={YOURDEVICE}
model_number={YOURDEVICE}
serial_number=
device_type=10-0050F204-5
config_methods=physical_display virtual_push_button
network={
ssid="XXXXX"
key_mgmt=NONE
priority=1
}
and it started with:
root@{yourdevice}:/ # cat system/etc/wifi/wpa_supplicant.conf
update_config=1
ctrl_interface=wlan0
eapol_version=1
ap_scan=1
fast_reauth=1
permissions:
root@{yourdevice}:/ # ls -l /data/misc/wifi
-rw-rw---- system wifi 21 2014-05-27 12:39 entropy.bin
drwxrwx--- wifi wifi 2014-05-27 12:39 sockets
-rw------- system system 33 2014-05-27 12:39 softap.conf
-rw-rw---- wifi wifi 272 2014-05-27 12:39 wpa_supplicant.conf
root@{yourboard}:/ # ls -l /data/misc/
drwxr-s--- system shell 2014-05-27 12:39 adb
drwxrwx--- bluetooth net_bt_stack 2014-05-27 12:39 bluedroid
drwxrwx--- system system 2014-05-27 12:39 bluetooth
drwxrwx--- dhcp dhcp 2014-05-27 12:39 dhcp
drwxrwx--x system system 2014-05-27 12:39 keychain
drwx------ keystore keystore 2014-05-27 12:39 keystore
drwx------ media media 2014-05-27 12:39 media
drwxrwx--- system radio 2014-05-27 12:39 radio
drwxrwx--- system radio 2014-05-27 12:39 sms
drwx------ system system 2014-05-27 12:39 systemkeys
drwxrwx--- system vpn 2014-05-27 12:39 vpn
drwxrwx--- wifi wifi 2014-05-27 12:39 wifi
drwxrwxr-x system system 2014-05-27 12:39 zoneinfo
root@{yourboard}:/ # ls -l /system/etc/wifi
-rw-rw---- wifi wifi 77 2014-05-27 12:39 wpa_supplicant.conf
root@{yourboard}:/ # ps | grep wpa
wifi 2555 1 3104 1876 c0103edc 401a4448 S /system/bin/wpa_supplicant
root@{yourboard}:/ # cat system/etc/permissions/platform.xml | grep -i wifi
<permission name="android.permission.ACCESS_WIFI_STATE" >
<group gid="wifi" />
<permission name="android.permission.CHANGE_WIFI_STATE" >
<group gid="wifi" />
<permission name="android.permission.WIFI" >
<group gid="wifi" />
root@{yourboard}:/ # cat system/etc/permissions/required_hardware.xml | grep wifi
<feature name="android.hardware.wifi" />
root@{yourboard}:/ # getprop | grep wifi
[net.tcp.buffersize.wifi]: [524288,1048576,2097152,262144,524288,1048576]
[ro.wifi.channels]: []
[wifi.interface]: [wlan0]
root@{yourboard}:/ # getprop | grep wlan
[dhcp.wlan0.dns1]: [192.168.1.1]
[dhcp.wlan0.dns2]: []
[dhcp.wlan0.dns3]: []
[dhcp.wlan0.dns4]: []
[dhcp.wlan0.domain]: []
[dhcp.wlan0.gateway]: [192.168.1.1]
[dhcp.wlan0.ipaddress]: [192.168.1.118]
[dhcp.wlan0.leasetime]: [86400]
[dhcp.wlan0.mask]: [255.255.255.0]
[dhcp.wlan0.pid]: [2689]
[dhcp.wlan0.reason]: [REBOOT]
[dhcp.wlan0.result]: [ok]
[dhcp.wlan0.server]: [192.168.1.1]
[dhcp.wlan0.vendorInfo]: []
[init.svc.dhcpcd_wlan0]: [running]
[wifi.interface]: [wlan0]
[wlan.driver.status]: [ok]
[wlan.interface]: [wlan0]
root@{yourboard}:/ # getprop | grep suppl
[init.svc.rtw_suppl]: [running]
root@{yourboard}:/ # cat /sys/kernel/debug/usb/devices
T: Bus=02 Lev=01 Prnt=01 Port=00 Cnt=01 Dev#= 2 Spd=480 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS=64 #Cfgs= 1
P: Vendor=0bda ProdID=8176 Rev= 2.00
S: Manufacturer=Realtek
S: Product=802.11n WLAN Adapter
S: SerialNumber=00e04c000001
C:* #Ifs= 1 Cfg#= 1 Atr=a0 MxPwr=500mA
I:* If#= 0 Alt= 0 #EPs= 4 Cls=ff(vend.) Sub=ff Prot=ff Driver=rtl8192cu
E: Ad=81(I) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=02(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=03(O) Atr=02(Bulk) MxPS= 512 Ivl=0ms
E: Ad=84(I) Atr=03(Int.) MxPS= 64 Ivl=125us
root@{yourboard}:/ # cat /sys/bus/usb/devices/2-1/product
802.11n WLAN Adapter
Useful commands:
disable wifi:
root@{yourboard}:/ # svc wifi disable
enable wifi:
root@{yourboard}:/ # svc wifi enable
open wifi settings panel:
root@{yourboard}:/ # am start -a android.intent.action.MAIN -n com.android.settings/.wifi.WifiSettings
manually starting supplicant with debug:
root@{yourboard}:/ # wpa_supplicant -Dnl80211 -iwlan0 -c/data/misc/wifi/wpa_supplicant.conf -dd -B
root@{yourboard}:/ # netcfg wlan0 up/down/dhcp
root@{yourboard}:/ # wpa_cli
> status
bssid=20:aa:4b:1b:a1:7c
ssid=ECTEST
id=0
mode=station
pairwise_cipher=NONE
group_cipher=NONE
key_mgmt=NONE
wpa_state=COMPLETED
ip_address=192.168.1.118
p2p_device_address=44:34:4c:8b:f2:10
address=44:34:4c:8b:f2:10
<3>CTRL-EVENT-STATE-CHANGE id=0 state=9 BSSID=20:aa:4b:1b:a1:7c SSID=ECTEST
<3>CTRL-EVENT-CONNECTED - connection to 20:aa:4b:1b:a1:7c completed (reauth) [id=0 id_str=]
> scan
cfg80211_rtw_scan(wlan0)
OK
> no packet in tx packet buffer (0)
survey done event(14) band:0 for wlan0
<3>CTRL-EVENT-SCAN-RESULTS
> scan_results
bssid / frequency / signal level / flags / ssid
20:aa:1b:1b:a1:7c 2437 -74 [WPS][ESS] ECTEST
00:1d:3e:bd:10:05 2457 -85 [WPA-PSK-TKIP][ESS] net02
68:7f:74:03:c6:be 2432 -59 [ESS] \x00\x00\x00\x00
c8:23:73:3f:05:71 2462 -66 [ESS] Nick's router. Hands off.
root@{yourboard}:/ # ifconfig wlan0
wlan0: ip 192.168.1.118 mask 255.255.255.0 flags [up broadcast running multicast]
root@{yourboard}:/ # dhcpcd wlan0
dhcpcd[3373]: version 5.5.6 starting
dhcpcd[3373]: wlan0: rebinding lease of 192.168.1.118
dhcpcd[3373]: wlan0: acknowledged 192.168.1.118 from 192.168.1.1
dhcpcd[3373]: wlan0: leased 192.168.1.118 for 86400 seconds
dhcpcd[3373]: forked to background, child pid 3405
root@{yourboard}:/ # netcfg
lo UP 127.0.0.1/8 0x00000049 00:00:00:00:00:00
eth0 UP 192.168.0.152/24 0x00001043 24:80:00:00:00:00
tunl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
sit0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
ip6tnl0 DOWN 0.0.0.0/0 0x00000080 00:00:00:00:00:00
wlan0 UP 192.168.1.118/24 0x00001043 44:34:4c:8b:f2:10
wlan1 DOWN 0.0.0.0/0 0x00001002 46:34:4c:8b:f2:10
Good luck with it and please let me know if you need more info.
problem/solution:
if you get this problem:
E/wpa_supplicant( 3159): Could not set interface wlan0 flags (UP): Unknown error 132
solution:
missing rfkill, error 132 means "operation not possible due to RFkill"
vim kernel_imx/arch/arm/mach-mx6/board-mx6sl_{yourboard}.c
static int mx6sl_shd_bt_power_change(int status){return 0;}
static struct platform_device mxc_bt_rfkill = {
.name = "mxc_bt_rfkill",
};
static struct imx_bt_rfkill_platform_data mxc_bt_rfkill_data = {
.power_change = mx6sl_shd_bt_power_change,
};
/* init function */
static void __init {yourboard}_init(void){
...
mxc_register_device(&mxc_bt_rfkill, &mxc_bt_rfkill_data);
}
problem:
E/WifiHW ( 2488): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": No such file or directory
solution:
setup correctly in init.rc and init.freescale.rc scripts wifi and wpa_supplicant permissions and services.
Hi All,
I am working to bring up RealTeck USB wifi dongel on android 4.3 and kernel 3.0.35 below are steps I followed :
1) I am building drivers as modules, copying them to /system/lib/modules/ and after that I added below lines in init.rc before wpa_supplicant service start.
insmod /system/lib/modules/cfg80211.ko
insmod /system/lib/modules/mac80211.ko
insmod /system/lib/modules/rtlwifi.ko
insmod /system/lib/modules/rtl8192c-common.ko
insmod /system/lib/modules/rtl8192cu.ko
2)wlan0 interface is creating successfully in /sys/class/net/wlan0.
3) After that I try to run below commands :
root@sabresd_6dq:wpa_supplicant -Dnl80211 -iwlan0 -c/data/misc/wifi/wpa_supplicant.conf -dd -B ---> success
root@sabresd_6dq: wpa_cli ----> Able to scan the devices form command line .
But if I try to do from application I am getting below errors:
E/WifiHW ( 2514): Unable to open connection to supplicant on "/data/system/wpa_supplicant/wlan0": Connection refused
D/BluetoothAdapter( 2755): 1101306992: getState() : mService = null. Returning STATE_OFF
I/wpa_supplicant( 3163): Successfully initialized wpa_supplicant
I/wpa_supplicant( 3163): rfkill: Cannot open RFKILL control device
E/wpa_supplicant( 3163): nl80211: Could not configure driver to use managed mode
E/wpa_supplicant( 3163): Could not read interface p2p0 flags: No such device
E/wpa_supplicant( 3163): p2p0: Failed to initialize driver interface
kindly help me to solve issues.
Thanks In Advance,
Ranganath TM
Hello Ranganath,
You need to run wpa_supplicant as service (in init.rc or init.xxxxx.rc script).
Do you need rf kill ?
We removed it completely from our android system.
BR,
Zoran