Dear all
Ubuntu was compiled from the imx_android442_r1. The compiled results generated file (boot.img, recovery.img, system.img, u-boot.bin, u-boot-mx6q.bin).
In MFGTOOL u-boot-6q.bin why I need to compile once and "mx" is not attached to the download . It will pass an incorrect setting of the .bashrc file ?
thank.
Hi kim
difference between u-boot.imx and u-boot.bin is described in
https://github.com/Freescale/u-boot-fslc/blob/patches-2014.10/doc/README.imximage
for creating SD on your Linux host :
dd if=u-boot.imx of=/dev/mmcblk0 conv=notrunc seek=2 bs=512
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Deare Freescale
How do I change then compiled using the MFG TOOL To make a u-boot.bin for download to eMMC memory?
Thank.