why MLO is not required in freescale

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why MLO is not required in freescale

718 Views
pushpachennuru
Contributor I

Hi,

               why MLO is not using for the i.mx6

           AS i know MLO is used to load u-boot into dd r ram in that case i.mx6 boot rom code consist ddr ram? or  where does u-boot is copied. how it loads the kernel.?

Thanks & Regards,

pushpa teja.c

Labels (2)
0 Kudos
1 Reply

462 Views
igorpadykov
NXP Employee
NXP Employee

Hi pushpa

boot process is described in Chapter 8 System Boot

i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

For Uboot one can look at app note

U-Boot for i.MX51 Based Designs

http://cache.freescale.com/files/dsp/doc/app_note/AN4173.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos