why IMX8QM CPU MEK board used two PMIC of "SPF-29420_C5" schematic?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why IMX8QM CPU MEK board used two PMIC of "SPF-29420_C5" schematic?

750件の閲覧回数
chunqiaohe
Contributor II

Hello NXP engineer,

   I download the reference design file named  "SPF-29420_C5 of IMXQM CPU board , in the design, i found IMX8 CPU used to PMIC to supply. I check the imx8 spc,  one PMIC of PF8100 have seven buck channels(buck1~buck7) and the power current capacity of each channel cat meet the requirement of  IMX8QM's power branch consumption, so why the sch design need to use two PF8100 chips?

thanks!
imx8qm power consumption.png
PMIC.png

0 件の賞賛
返信
2 返答(返信)

745件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chunqiaohe

 

one pmic may be insufficient according to requirements in Table 10. Maximum supply currents

i.MX 8QuadMax Automotive and Infotainment Applications Processors

 

Best regards
igor

0 件の賞賛
返信

742件の閲覧回数
chunqiaohe
Contributor II

Dear igor,

    thanks for your replay , i also notice the Table-10 " Maximum supply currents", but in this page have a note " Some of the numbers shown in this table are based on the companion regulator limits and not actual use cases. Work is in progress to provide use case–based numbers in future data sheet releases "
    so i can't confirm whether is it accurate, and i want to reduce a product's cost, if  you advise follow the maximum supply current vlaue of the Table-10. i will do it.

   thanks!

 

0 件の賞賛
返信