who have the patch about pcie bus on the linux 3.0.35?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

who have the patch about pcie bus on the linux 3.0.35?

643 Views
xiuqingchang
Contributor I

who have the patch about pcie bus on the linux 3.0.35?

I work on the imx6q ,when i debug pcie bus on the linux 3.0.35,there is some problem,however on the linux3.10.17,it's ok,so i want to have the patch about pcie on the linux3.0.35,or tell me the difference between linux 3.0.35 and linux3.10.17 about pcie bus;thanks

0 Kudos
Reply
1 Reply

544 Views
art
NXP Employee
NXP Employee

There is no separate patch for that since some problems of the 3.0.35 BSP (not only related with PCIe) were on the kernel level and newer kernel should be used to fix them.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply