which toch screen display can support i.MX 6SoloX SABRE Development Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which toch screen display can support i.MX 6SoloX SABRE Development Board

390 Views
anilchowdary
Contributor II

HI Nxp,

 I want work with 4.3 touch screen display with sabersd board (MCIMX6SX-SDB),

1.can any one suggest which  touch screen display (4.3 inch diaply)  will supports Sabersd board and what is the interface?

2.In the this board touch screen display drivers are enabled are not? if no, please can you share the how to enable particular (which you suggested) display driver?

Thanks for your replay

Regards

-Anil

Labels (1)
0 Kudos
1 Reply

330 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anil

supported MCIMX-LVDS1 and its specs are provided on

https://community.freescale.com/message/331832#331832

also it is supported in linux, please refer to attached Linux documents.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos