where to get Freescale L2.6.35_11.05.01_ER_source_bundle.tar.gz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where to get Freescale L2.6.35_11.05.01_ER_source_bundle.tar.gz

1,375 Views
MadhusudhananRa
Contributor I

Hi Guys,

Is there any chance I can download  L2.6.35_11.05.01_ER_source_bundle.tar.gz

While I check the Freescale IMX53 QSB product page, I can only get the latest bsp which is

L2.6.35_11.09.01_ER_source_bundle.tar.gz

To reproduce some issues, I need to get back to the same environment as in the L2.6.35_11.05.01_ER and with same versions of packages.

Regards,

Madhu

Labels (1)
0 Kudos
5 Replies

881 Views
VladanJovanovic
NXP Employee
NXP Employee

You can download it from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...

You'll find it under "Board Support Packages"

0 Kudos

881 Views
Yuri
NXP Employee
NXP Employee

If the 11.05.01 is needed - I can try for forward it via the TransWeb (~700 MB).
Please create Service Request via the Web (www.freescale.com) and let me know its number. 

0 Kudos

881 Views
Yuri
NXP Employee
NXP Employee

Sorry, many versions may be found on internal Freescale resource, but I cannot find just
11.05.01 on the (external) Web. 

0 Kudos

881 Views
MadhusudhananRa
Contributor I

Hi Yuri,

It works, thanks, by the by, is there any archive page from freescale where we can download all the previous versions.

Regards

Madhu

0 Kudos