Hi Guys,
Is there any chance I can download L2.6.35_11.05.01_ER_source_bundle.tar.gz
While I check the Freescale IMX53 QSB product page, I can only get the latest bsp which is
L2.6.35_11.09.01_ER_source_bundle.tar.gz
To reproduce some issues, I need to get back to the same environment as in the L2.6.35_11.05.01_ER and with same versions of packages.
Regards,
Madhu
You can download it from:
You'll find it under "Board Support Packages"
If the 11.05.01 is needed - I can try for forward it via the TransWeb (~700 MB).
Please create Service Request via the Web (www.freescale.com) and let me know its number.
Sorry, many versions may be found on internal Freescale resource, but I cannot find just
11.05.01 on the (external) Web.
Hi Yuri,
It works, thanks, by the by, is there any archive page from freescale where we can download all the previous versions.
Regards
Madhu