where is weston.ini default setting ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is weston.ini default setting ?

3,002件の閲覧回数
Ichi_
Contributor I

Hi All,

Environment:

kernel:5.4

evk:imx8mq-evk

bitbake imx-image-full

sn65dsi83 mipi to lvds

 

Question:

I can see the image out on the panel by modified /etc/xdg/weston/weston.ini

drm-device=card0->card2 after boot.

 

May I ask Where to modify the default is card2 in my bitbake imx-image-ful build image?

 

 

 

 

0 件の賞賛
返信
2 返答(返信)

2,979件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The weston. ini configuration file is searched for in one of the following places when the server is started: $XDG_CONFIG_HOME/weston. ini (if $XDG_CONFIG_HOME is set) $HOME/. config/weston.

You fail about the card2 is turned out to be a missing hardware configuration in the device tree.

 

Regards

0 件の賞賛
返信

2,900件の閲覧回数
Ichi_
Contributor I

Hi @Bio_TICFSL 

 

The panel can see the image, so the device tree should be set correctly.

Do you know which path of weston.ini needs to be modified to card2?

That is, the drm-device value at boot after burning is card2.

Thanks.

 

 

0 件の賞賛
返信