where is dts file for imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

where is dts file for imx6

跳至解决方案
2,115 次查看
yeyue
Contributor II

I build ltib for imx6 on ubuntu12.04 using package L3.0.35_4.1.0_130816_source.tar.gz

and it can work to produce uboot,kernel image,rootfs

but I can't find any dts files in  rpm/BUILD/linux-3.0.35/arch/arm/boot/

does anyone have ever met this problem?

thanks

0 项奖励
回复
1 解答
1,737 次查看
Yuri
NXP Employee
NXP Employee

Hello,

NXP BSP L3.0.35 does not support the Device Tree.


Have a nice day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,738 次查看
Yuri
NXP Employee
NXP Employee

Hello,

NXP BSP L3.0.35 does not support the Device Tree.


Have a nice day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,737 次查看
yeyue
Contributor II

Thanks.

If BSP L3.0.35 does not support the Device Tree,

so I need to update BSP for other version?

otherwise how can I change the pinctr in dts file?

0 项奖励
回复
1,737 次查看
Yuri
NXP Employee
NXP Employee

Hello,

You may try the recent BSP L3.14.52.

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS

Summary Page :

i.MX 6 Series Software and Development Tool|NXP

Please follow recommendations of "Freescale_Yocto_Project_User's_Guide.pdf"


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复