where is a start timing at "180ms" of AUTO_RESTART bit?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is a start timing at "180ms" of AUTO_RESTART bit?

608件の閲覧回数
t-iishii
Contributor II

Hi community,

I have one question about AUTO_RESTART bit of HW_RTC_PERSISTENT0 register on i.MX28.

In Reference Manual of i.MX28, Description of AUTO_RESTART bit is following.

17 AUTO_RESTART "Set to one to enable the chip to automatically power up approximately 180 ms after powering down."

In this comment, where is a start timing at "180ms"?

Best regards,

Ishii.

ラベル(1)
0 件の賞賛
3 返答(返信)

458件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

start will be from moment when power supplies become turned off.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

458件の閲覧回数
t-iishii
Contributor II

Hello igor,

Thank you for your quick response.

You say that if Power source is only DCDC_BAT,

"turned off" timing is that system detect DCDC_BAT low level and start brownout sequence.

Is it correct?

If so, does it have some method to detect start timing by software or external signal?

Best regards,

Ishii.

0 件の賞賛

458件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

 

I said : "start will be from moment when power supplies become turned off."

I am afraid there is no way detect start timing by software or external signal.

 

Best regards
igor

0 件の賞賛