where can i find i.MX31 PDK 1.5 Linux User’s Guide

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where can i find i.MX31 PDK 1.5 Linux User’s Guide

1,020 Views
stevenshan
Contributor II

The belows is from Developing an Application for the i.MX Devices on the Linux Platform ,but i can not search i.MX31 PDK 1.5 Linux User’s Guide ,where can i find it?

If the user requires any help to set up the prerequisites, refer to the Linux BSP documents. For example,for setting up the i.MX31 PDK, refer to the i.MX31 PDK 1.5 Linux User’s Guide (926-77208), which is available in the BSP tarball that resides in the /doc/ directory.

Labels (2)
0 Kudos
Reply
2 Replies

881 Views
stevenshan
Contributor II

I had found the file below,i think is the file  i.MX31 PDK 1.5 Linux User’s Guide

i.MX31 3-Stack Platform Linux SDK

Standard Release Package User’s Guide

Document Number: 926-77208

Rev. 1.2

02/2008

0 Kudos
Reply

881 Views
igorpadykov
NXP Employee
NXP Employee

it is located on i.MX31 PDK product page, below full links:

Supporting Information (4)

i.MX35 PDK Linux Documentation Bundle (REV 2009.12)

http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx35-product-developm...

Board Support Packages (2)

Linux 2.6.31 Source Code Files 2009.12 Release support i.MX23, i.MX25, i.MX35, i.MX51. (REV 2009.12)

http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx35-product-developm...

~igor

0 Kudos
Reply