where can I get imx6 source "L3.0.35_1.1.0_121218_source.tar.gz"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where can I get imx6 source "L3.0.35_1.1.0_121218_source.tar.gz"

1,086 Views
dayuan
Contributor I

Where can I get imx6 source "L3.0.35_1.1.0_121218_source.tar.gz"?

The lastest is L3.0.35_4.1.0_130816_source.tar.

But I want to get the older source.

Labels (1)
0 Kudos
2 Replies

458 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi da yuan,

I saw that you also create the same question on our Chinese website, and I already give you reply there. The version of L3.0.35_1.1.0_121218_source.tar.gz BSP is old and do not exist on website. So here you can choose the L3.0.35_4.1.0 BSP, the downloading link is :http://www.freescale.com/product ... ab=Design_Tools_Tab​.

Hope this can help you.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

458 Views
dayuan
Contributor I

Thanks for you help.

I want to do fast boot imx6 with lvds .

I follow by Linux Fast Boot on i.MX6 Sabresd Board,but my boot time is more than 3 sec.

I use source  L3.0.35_4.1.0 BSP,Linux Fast Boot on i.MX6 Sabresd Board  use L3.0.35_1.1.0 BSP.

Maybe there are something different with L3.0.35_1.1.0 BSP.

So I want to download L3.0.35_1.1.0 BSP to try.

0 Kudos