what to initialize in uboot - general recommendation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what to initialize in uboot - general recommendation

Jump to solution
1,498 Views
nexy_sm
Contributor II

Hi all,

I am working on a custom board based on imx6 and sabreauto. This rather not a specific question but more asking for an advice and best practice. How to divide what should be initialized in uboot and what should be initialized later by Linux. How do you divide that in your designs?

Thank you

Labels (2)
0 Kudos
Reply
1 Solution
1,379 Views
joanxie
NXP TechSupport
NXP TechSupport

suggest you can refer to the source code, for uboot, you can refer to the "/git/board/freescale/", choose the board you need, you can find what hardware configuration in the uboot, then you can refer to the dts file in the kernel, the path is arch/arm/boot/dts, choose the board dts file, if you need to change something, you can refer the dts file in the kernel source code

View solution in original post

0 Kudos
Reply
1 Reply
1,380 Views
joanxie
NXP TechSupport
NXP TechSupport

suggest you can refer to the source code, for uboot, you can refer to the "/git/board/freescale/", choose the board you need, you can find what hardware configuration in the uboot, then you can refer to the dts file in the kernel, the path is arch/arm/boot/dts, choose the board dts file, if you need to change something, you can refer the dts file in the kernel source code

0 Kudos
Reply