uboot中的lcd参数: video=mxcfb0:dev=lcd,HUD-WVGA,if=RGB24,bpp=24
设备树:mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "lcd";
interface_pix_fmt = "RGB24";
mode_str ="HUD-WVGA";
default_bpp = <24>;
int_clk = <0>;
late_init = <0>;
status = "disabled";
};
lcd@0 {
compatible = "fsl,lcd";
ipu_id = <0>;
disp_id = <0>;
default_ifmt = "RGB24";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1>;
status = "okay";
};
在结合驱动文件: mxc_ipuv3_fb.c中的mxcfb_option_setup函数解析, 可以知道uboot中传递的参数bpp = 24用于确定fb_pix_fmt, 而uboot中的if = RGB24用于确定 interface_pix_fmt, 请问这两个有什么区别, 这个lcd屏与imx6硬件连接有关系吗?
Hi Edward
relationship with i.MX6Q hardware connections can be found in
sect.4.11.10.4 IPU Display Interface Signal Mapping i.MX6DQ Datasheet
http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igorpadykov
as you mentioned, my board hardware interface is as follows:
imx6 side lcd side
DISP0_DAT0 <---> B0
DISP0_DAT1 <---> B1
DISP0_DAT2 <---> B2
DISP0_DAT3 <---> B3
DISP0_DAT4 <---> B4
DISP0_DAT5 <---> B5
DISP0_DAT6 <---> B6
DISP0_DAT7 <---> B7
DISP0_DAT8 <---> G0
DISP0_DAT9 <---> G1
DISP0_DAT10 <---> G2
DISP0_DAT11 <---> G3
DISP0_DAT12 <---> G4
DISP0_DAT13 <---> G5
DISP0_DAT14 <---> G6
DISP0_DAT15 <---> G7
DISP0_DAT16 <---> R0
DISP0_DAT17 <---> R1
DISP0_DAT18 <---> R2
DISP0_DAT19 <---> R3
DISP0_DAT20 <---> R4
DISP0_DAT21 <---> R5
DISP0_DAT22 <---> R6
DISP0_DAT23 <---> R7
so in uboot args: video=mxcfb0:dev=lcd,HUD-WVGA,if=RGB24,bpp=24
if = RGB24 or if = BGR24?
Hi Igor,
Yes, I pass the parameter(if = RGB) in uboot. But, I write a test program to display blue, actually it display red. I am doubt whether I wrote the test program wrongly. As I mark below in red color, I use rgb data( b = 0x11111111; g = 0; r = 0; ) to fill mapped memory (*(fbp + location) = b; *(fbp + location + 1) = g; *(fbp + location + 2) = r;).
The test program is as follow:
#include <stdio.h>
#include <unistd.h>
#include <fcntl.h>
#include <sys/mman.h>
#include <linux/fb.h>
int main(void)
{
int fbfd = 0;
struct fb_var_screeninfo vinfo;
struct fb_fix_screeninfo finfo;
struct fb_cmap cmapinfo;
long int screensize = 0;
char *fbp = 0;
int x = 0, y = 0;
long int location = 0;
int b, g, r;
/* open /dev/fb0 */
fbfd = open("/dev/fb0", O_RDWR);
if (fbfd < 0) {
printf("ERR: open framebuffer device failed\n");
return -1;
}
printf("open framebuffer device successfully\n");
/* map the device to memory */
fbp = (char *)mmap(0, screensize, PROT_READ | PROT_WRITE, MAP_SHARED, fbfd, 0);
if ((-1 == (int)fbp)) {
printf("ERR: failed to map framebuffer device to memory\n");
return -1;
}
printf("success to map framebuffer device to memory\n");
b = 0x11111111; // blue
g = 0; // green
r = 0; // red
/* display the whole screen, and the pix is 480x240 */
vinfo.xoffset = 0; // Where we are going to put the pixel
vinfo.yoffset = 0;
// Figure out where in memory to put the pixel
for ( y = 0; y < 240; y++ )
for ( x = 0; x < 480; x++ ) {
location = (x+vinfo.xoffset) * (vinfo.bits_per_pixel/8) +
(y+vinfo.yoffset) * finfo.line_length;
if ( vinfo.bits_per_pixel == 32 ) { // 32bpp
*(fbp + location) = b; //blue
*(fbp + location + 1) = g; // green
*(fbp + location + 2) = r; // red
*(fbp + location + 3) = 0; // No transparency
} else if (vinfo.bits_per_pixel == 24) { //24bpp: r:g:b=8:8:8
*(fbp + location) = b;
*(fbp + location + 1) = g;
*(fbp + location + 2) = r;
}
}
munmap(fbp, screensize);
close(fbfd);
return 0;
}
Best regards
Edward
Hi Edward
had you adjusted lcd timings, sone example can be found on
https://community.nxp.com/thread/373763
Best regards
igor