what's the EPDC_STANDARD_MODE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what's the EPDC_STANDARD_MODE

Jump to solution
731 Views
yan2anfei
Contributor III

hi ,

The EPDC_STANDARD_MODE is  defined In the file of imx7d_epdc_v2_fb.c.

what's the feature in this mode ?

 

best regards!

0 Kudos
Reply
1 Solution
544 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Yan2,

The EPD function can be separated into two major asynchronous processes. The first is
the front end portion which is responsible for processing display updates. The second is
the function of driving waveforms to the TFT panel in order to update the screen contents
(the refresh operation).

With the EPDC_STANDARD MODE you are selecting the  Waveform mode. The EPDC provides a mechanism through its histogram analysis feature (which can be run as part of any frame/region processing operations)
to allow the SW driver to characterize the region/buffer in terms of gray-map content.

For example, EPDC can determine if the update region (considering only those pixels undergoing a transition) contains only 2, 4, 8 or 16 gray levels, HW can automatically select waveform mode according to a programmed LUT holding
mapping between grey level and waveform mode. SW driver can also manually
choose the appropriate waveform update mode (e.g., when doing an update to repair
ghosting artifacts).

If you want to see further details please refer to section 13.6.3.4.2 Panel Architecture Configuration of the i.MX7D Reference Manual.

Have a nice day!

Jaime

View solution in original post

0 Kudos
Reply
1 Reply
545 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Yan2,

The EPD function can be separated into two major asynchronous processes. The first is
the front end portion which is responsible for processing display updates. The second is
the function of driving waveforms to the TFT panel in order to update the screen contents
(the refresh operation).

With the EPDC_STANDARD MODE you are selecting the  Waveform mode. The EPDC provides a mechanism through its histogram analysis feature (which can be run as part of any frame/region processing operations)
to allow the SW driver to characterize the region/buffer in terms of gray-map content.

For example, EPDC can determine if the update region (considering only those pixels undergoing a transition) contains only 2, 4, 8 or 16 gray levels, HW can automatically select waveform mode according to a programmed LUT holding
mapping between grey level and waveform mode. SW driver can also manually
choose the appropriate waveform update mode (e.g., when doing an update to repair
ghosting artifacts).

If you want to see further details please refer to section 13.6.3.4.2 Panel Architecture Configuration of the i.MX7D Reference Manual.

Have a nice day!

Jaime

0 Kudos
Reply