what is value of GPIO source/sink current per pin on i.MX6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what is value of GPIO source/sink current per pin on i.MX6?

2,061 次查看
nirmalakunwar
Contributor I

What is the current limit on single GPIO output which it can source / sink without any issue

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

1,312 次查看
art
NXP Employee
NXP Employee

The GPIO buffer load capacity is not specified in units of current. It is specified in terms of buffer drive strength or output impedance. For example, refer to the Section 4.8.1 "GPIO Output Buffer Impedance" of the i.MX 6Dual/6Quad  Applications Processors for Consumer Products Data Sheet Rev.4 document, available on the processor's Documentation web page:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Also, the total load current and power dissipation should be taken into account when calculating the GPIO power budget.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复