what is the sequence of DISP0_DATx map to RGB888?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

what is the sequence of DISP0_DATx map to RGB888?

跳至解决方案
2,372 次查看
翔李
Contributor IV

HI,BOSS,

0: I want to use RGB888 to display video.

1:what is the sequence of the RGB888 to the pin of IMX6Q? it is mean,which of the DISP0_DATx map  to R[0:7]?Also to G[0:7],B[0:7]? And can the map change difference sequence in other order between DISP0_DATx and RGB[0:7]?

THANKS.

pastedImage_1.png

0 项奖励
回复
1 解答
2,061 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 4.11.10.4 (IPU Display Interface Signal Mapping) of the Datasheet.

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

在原帖中查看解决方案

5 回复数
2,061 次查看
honglinguo
Contributor I

pastedImage_1.png

Hello,

      Please tell me the difference between these documents.

Thanks!

0 项奖励
回复
2,061 次查看
翔李
Contributor IV

A:AUTOMOTIVE

C:CONSUMER

I:INDUSTRIAL

2,061 次查看
honglinguo
Contributor I

thanks!

0 项奖励
回复
2,062 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 4.11.10.4 (IPU Display Interface Signal Mapping) of the Datasheet.

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

2,061 次查看
翔李
Contributor IV

Thanks so much.

0 项奖励
回复