what is the sequence of DISP0_DATx map to RGB888?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the sequence of DISP0_DATx map to RGB888?

ソリューションへジャンプ
2,624件の閲覧回数
翔李
Contributor IV

HI,BOSS,

0: I want to use RGB888 to display video.

1:what is the sequence of the RGB888 to the pin of IMX6Q? it is mean,which of the DISP0_DATx map  to R[0:7]?Also to G[0:7],B[0:7]? And can the map change difference sequence in other order between DISP0_DATx and RGB[0:7]?

THANKS.

pastedImage_1.png

0 件の賞賛
返信
1 解決策
2,313件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 4.11.10.4 (IPU Display Interface Signal Mapping) of the Datasheet.

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

元の投稿で解決策を見る

5 返答(返信)
2,313件の閲覧回数
honglinguo
Contributor I

pastedImage_1.png

Hello,

      Please tell me the difference between these documents.

Thanks!

0 件の賞賛
返信
2,313件の閲覧回数
翔李
Contributor IV

A:AUTOMOTIVE

C:CONSUMER

I:INDUSTRIAL

2,313件の閲覧回数
honglinguo
Contributor I

thanks!

0 件の賞賛
返信
2,314件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 4.11.10.4 (IPU Display Interface Signal Mapping) of the Datasheet.

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX6DQCEC.pdf 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

2,313件の閲覧回数
翔李
Contributor IV

Thanks so much.

0 件の賞賛
返信