what is the ic of 4cvbs_camera in for imx6q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the ic of 4cvbs_camera in for imx6q?

501 Views
翔李
Contributor IV

hi,

1:what is the  ic of 4cvbs_camera in for imx6q in FSL's demo,also support for driver?

Is it tw2866 or te2867?or others.Please give me some links or files for 4-cvbs_camera input for imx6q demo.

Thanks.

Tags (1)
0 Kudos
2 Replies

367 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please look at below link with example driver for Maxim MAX9286, it was verified working

on iMX6DQ SabreAuto board. The input to MAX9286 is four 720P30 cameras.

Also verified camera boards:

    (1) Onsemi AR0140+AP0101+MAX9271 boards.

    (2) OmniVision OV10635+MAX9271 boards.

https://community.freescale.com/docs/DOC-328548

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

367 Views
翔李
Contributor IV

hi,

Thanks.

1:I prefer to use csi0 to connect 4_csi0.jpgcvbs_camera in. So the same question.

0 Kudos