what is the effect of the resistor in the FB circuit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the effect of the resistor in the FB circuit?

1,182 Views
翔李
Contributor IV

HI

  Athough my question is not about NXP's IC,but please help me to slove it,thanks so much.

what is the effect of the resistor in the FB circuit,the green rectangle R193?

And also what is the effect of the circuit red rectangle signal pwm_cut0?

pastedImage_2.png

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

969 Views
art
NXP Employee
NXP Employee

Since I don't see the whole schematic, I cannot make any definite conclusions. I can only suppose that the whole circuit (both red and green rectangles) is meant to add some small bias voltage, taken from the PWM_OUT0 signal and then rectified on the R6/C225 circuit, to the feedback point to control the DVDD_CORE voltage with an external PWM (the source of the PWM_OUT0 signal).

Please note that this is only my own supposition and I cannot claim that it is true in any way.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply