what is the difference betweent USDHC4 and USDHC3(mx6-SDP)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the difference betweent USDHC4 and USDHC3(mx6-SDP)?

Jump to solution
1,804 Views
cody
Contributor II

I  am  reading  latest source codes(L3.0.35_4.1.0_130816_source)   in linux/arch/arm/mach-mx6/board-mx6dl_sabresd.h...now..

/* USDHC3 */

MX6DL_PAD_SD3_CLK__USDHC3_CLK_50MHZ,

MX6DL_PAD_SD3_CMD__USDHC3_CMD_50MHZ,

MX6DL_PAD_SD3_DAT0__USDHC3_DAT0_50MHZ,

MX6DL_PAD_SD3_DAT1__USDHC3_DAT1_50MHZ,

MX6DL_PAD_SD3_DAT2__USDHC3_DAT2_50MHZ,

MX6DL_PAD_SD3_DAT3__USDHC3_DAT3_50MHZ,

MX6DL_PAD_SD3_DAT4__USDHC3_DAT4_50MHZ,

MX6DL_PAD_SD3_DAT5__USDHC3_DAT5_50MHZ,

MX6DL_PAD_SD3_DAT6__USDHC3_DAT6_50MHZ,

MX6DL_PAD_SD3_DAT7__USDHC3_DAT7_50MHZ,

/* SD3_CD */

MX6DL_PAD_NANDF_D0__GPIO_2_0,

/* SD3_WP */

MX6DL_PAD_NANDF_D1__GPIO_2_1,

/* USDHC4 */

MX6DL_PAD_SD4_CLK__USDHC4_CLK_50MHZ,

MX6DL_PAD_SD4_CMD__USDHC4_CMD_50MHZ,

MX6DL_PAD_SD4_DAT0__USDHC4_DAT0_50MHZ,

MX6DL_PAD_SD4_DAT1__USDHC4_DAT1_50MHZ,

MX6DL_PAD_SD4_DAT2__USDHC4_DAT2_50MHZ,

MX6DL_PAD_SD4_DAT3__USDHC4_DAT3_50MHZ,

MX6DL_PAD_SD4_DAT4__USDHC4_DAT4_50MHZ,

MX6DL_PAD_SD4_DAT5__USDHC4_DAT5_50MHZ,

MX6DL_PAD_SD4_DAT6__USDHC4_DAT6_50MHZ,

MX6DL_PAD_SD4_DAT7__USDHC4_DAT7_50MHZ,

So   the  difference  betweent   USDHC4  and  USDHC3  is  that  there are  SD3_WP and SD3_CD in  USDHC3   while   USDHC4    do   not  have.

So   Does   USDHC3   used  for  SD card  while  USDHC4   used  for  eMMC?

Labels (2)
1 Solution
1,308 Views
justin_jiang
NXP Employee
NXP Employee

Yes. The WP and CD pin can be configured by IOMUX.

View solution in original post

1 Reply
1,309 Views
justin_jiang
NXP Employee
NXP Employee

Yes. The WP and CD pin can be configured by IOMUX.