I am reading latest source codes(L3.0.35_4.1.0_130816_source) in linux/arch/arm/mach-mx6/board-mx6dl_sabresd.h...now..
/* USDHC3 */
MX6DL_PAD_SD3_CLK__USDHC3_CLK_50MHZ,
MX6DL_PAD_SD3_CMD__USDHC3_CMD_50MHZ,
MX6DL_PAD_SD3_DAT0__USDHC3_DAT0_50MHZ,
MX6DL_PAD_SD3_DAT1__USDHC3_DAT1_50MHZ,
MX6DL_PAD_SD3_DAT2__USDHC3_DAT2_50MHZ,
MX6DL_PAD_SD3_DAT3__USDHC3_DAT3_50MHZ,
MX6DL_PAD_SD3_DAT4__USDHC3_DAT4_50MHZ,
MX6DL_PAD_SD3_DAT5__USDHC3_DAT5_50MHZ,
MX6DL_PAD_SD3_DAT6__USDHC3_DAT6_50MHZ,
MX6DL_PAD_SD3_DAT7__USDHC3_DAT7_50MHZ,
/* SD3_CD */
MX6DL_PAD_NANDF_D0__GPIO_2_0,
/* SD3_WP */
MX6DL_PAD_NANDF_D1__GPIO_2_1,
/* USDHC4 */
MX6DL_PAD_SD4_CLK__USDHC4_CLK_50MHZ,
MX6DL_PAD_SD4_CMD__USDHC4_CMD_50MHZ,
MX6DL_PAD_SD4_DAT0__USDHC4_DAT0_50MHZ,
MX6DL_PAD_SD4_DAT1__USDHC4_DAT1_50MHZ,
MX6DL_PAD_SD4_DAT2__USDHC4_DAT2_50MHZ,
MX6DL_PAD_SD4_DAT3__USDHC4_DAT3_50MHZ,
MX6DL_PAD_SD4_DAT4__USDHC4_DAT4_50MHZ,
MX6DL_PAD_SD4_DAT5__USDHC4_DAT5_50MHZ,
MX6DL_PAD_SD4_DAT6__USDHC4_DAT6_50MHZ,
MX6DL_PAD_SD4_DAT7__USDHC4_DAT7_50MHZ,
So the difference betweent USDHC4 and USDHC3 is that there are SD3_WP and SD3_CD in USDHC3 while USDHC4 do not have.
So Does USDHC3 used for SD card while USDHC4 used for eMMC?
解決済! 解決策の投稿を見る。
Yes. The WP and CD pin can be configured by IOMUX.