what is the boot argument to load UBUNTU binary image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the boot argument to load UBUNTU binary image

1,040件の閲覧回数
VadivelmuruganR
Contributor I

Dear All,

          I want to launch iMX50_Ubuntu_Demo_Image.bin on i.MX50 QSB ,I can able to copy by using DD

command .but freescale did not given any boot parameters ,If any one knows it would be appreciatable.

Thanks

Muruagn 

タグ(1)
0 件の賞賛
返信
1 返信

981件の閲覧回数
PeterChan
NXP Employee
NXP Employee

The boot parameters are already set in the demo image. Just dd the the image to your SD card from the first sector and the card is ready to boot. By default, the display device is "hdmi".

To inspect and change the boot parameter, just hit any key in your serial console to stop the auto boot countdown and then type the command "printenv".

0 件の賞賛
返信