what is the approach(procedure) to do FOTA in imxRT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the approach(procedure) to do FOTA in imxRT1064

1,547 Views
karthik1
Contributor I

Hi sir,

1.Please suggest me the approach to do FOTA update using Ethernet (application program to download the firmware  into external flash hyperflash/ QSPI NOR flash )  in imxRT1064 board.?

2.Amazon FreeRTOS  OTA demo code is supported for imxRT1050 but not given SDK Amazon FreeRTOS  OTA demo code for imxRT1064 ?

3. Any suggestion using secondary bootloader to do FOTA?

4. How to bootloader programming for FOTA in imxRT1064?

thanks and regards

Karthik 

 

Labels (1)
0 Kudos
Reply
2 Replies

1,325 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Karthik,

 

I am sorry for the late reply.

 

I highly recommend you to check the ota _demo_enet example from the RT1060 SDK. Even though support may be limited as this is not officially supported in the SDK, I suggest you to check the community document below that explains how you can run demos  on the i.MXRT1064-EVK with just a few modification to the RT1060 projects.

 

eIQ on i.MX RT1064 EVK 

 

I hope this helps you.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,325 Views
karthik1
Contributor I

Hi  felipe garcia,

thank you for your reply

thanks and regards 

Karthik  N E

0 Kudos
Reply