Dear NXP team.
I have a "IMX6DQ6SDLSRM_security.pdf" doc file.
- Document Number: IMX6DQ6SDLSRM Rev. 0, 03/2013
Question 1. I can not find what is the JRSDIDR and what does it mean in the doc file.
B.2.6 Job Ring Registers
This section describes registers found in each of the job rings. A functional description of
the job rings can be found in the “Cryptographic Acceleration and Assurance Module
(CAAM)” chapter.
If the job ring is allocated to TrustZone SecureWorld (JRSDIDR TZ=1), then the job ring
registers associated with this ring may only be written via a bus transaction that has ns=0.
Transactions with ns=1 for job rings owned by TrustZone SecureWorld will be ignored.
Question 2. Input/Output Ring Base Address Register
There are each 2 Input/Output Ring Base Address Register .
- IRBAR0, IRBAR1
- ORBAR0, ORBAR01
What is the different of IRBAR0, IRBAR1 and ORBAR0, ORBAR01 ?
- ex) IRBAR0 is for TrustZone SecureWorld and IRBAR1 is for TrustZone Non-SecureWorld ?
Best regards,
MyungJin Hwang
I really don't understand it.
2 Job rings mean "input job ring" and "output job ring" right?
and 2 copies of the register is "JR0" "JR1"?
for what, there are 2 copies of the register?
could you explain easily?
Thanks
Hi MyungJin
please look at sect.1.8.1.4 Job Ring SDID Register (JRSDIDR)
LS1021ASECRM, QorIQ LS1021A Security (SEC) Reference Manual - Reference Manual (REV 0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------