Hi,
I am planning to boot from NOR flash on my sabre sd platform(imx6q) and as such
I copied the u-boot.bin to NOR flash from on board SD card.But could not find DIP switch settings for booting from NOR flash.
could pls any one know the settings?
SPI NOR programming:log
=====================
MX6Q SABRESD U-BootPS > mmc dev 2
mmc2 is current device
MX6Q SABRESD U-BootPS > mmc read $(loadaddr) 0 0x200
MMC read: dev # 2, block # 0, count 512 ... 512 blocks read: OK
MX6Q SABRESD U-BootPS > sf probe 0
JEDEC ID: 0x20:0x20:0x16
4096 KiB M25P32 - 4MB at 0:0 is now current device
MX6Q SABRESD U-BootPS > sf erase 0 0x40000
MX6Q SABRESD U-BootPS > sf write $(loadaddr) 0 0x40000
..............................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................................
...................................................................SUCCES
Thanks in advance,
suresh.
解決済! 解決策の投稿を見る。
Yes, it is possible to use "normal" u-boot for SD booting.
As for details, please look at section 5.3 (Multi-environment store device) of "uboot_mx6x.pdf".
Table 8-22 (Serial ROM Boot eFUSE Descriptions) of the i.MX6(Q) Reference
Manual (RM) shows configuration for SPI boot :
BOOT_CFG1[7:4] = 0011 (Boot from Serial ROM).
BOOT_CFG4[5:4] = 00 (CS#0).
BOOT_CFG4[3] defines number of address bytes.
BOOT_CFG4[2:0] = 000 (ECSPI-1).
Basically such BOOT_CFG configuration may be provided on the MX6 SDP, but the
problem arises to pin multiplexing : for example CSPI1_clk is connected to i.MX6
KEY_COL0 pin, and according to Table 8-25 (SPI IOMUX Pin Configuration) of the
RM, such pin multiplexing (ECSPI-1) is not supported for SPI NOR boot.
Hi Yuri,
Thanks you for the help.
actually the sabre platform has SW6 dip switch having 8 switched(D1-D8) and the SABRE_SD_User_Guide_L3.0.35_1.1.0 has settings for SD card booing on slot 1and 3, SATA, eMMC but no seeings for SPI-NOR flash booting. for instance below is a setting for SD card boot.
Table 4-2. the boot switch setup for SD3 boot (J507)
Switch D1 D2 D3 D4 D5 D6 D7 D8
SW6 OFF ON OFF OFF OFF OFF ON OF
I even wonder if we need to build u-boot with special configuartion settings or just can use normal u-boot.bin built for SD card booting.
Thanks,
Suresh.
Yes, it is possible to use "normal" u-boot for SD booting.
As for details, please look at section 5.3 (Multi-environment store device) of "uboot_mx6x.pdf".