what are the pins to be connected in schematic for giving a provision for boot from Nand flash/ SD Card / Internal memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what are the pins to be connected in schematic for giving a provision for boot from Nand flash/ SD Card / Internal memory

512 Views
muralikrishna
Contributor I

In I.MX6 Quad processor, what are hardware pins to be used in the schematic for selecting boot options from NAND Flash / SD Card / Internal.

Labels (1)
0 Kudos
1 Reply

411 Views
igorpadykov
NXP Employee
NXP Employee

Hi Murali

please look at SPF-27142  p.3, 9

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos