what are the pins to be connected in schematic for giving a provision for boot from Nand flash/ SD Card / Internal memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what are the pins to be connected in schematic for giving a provision for boot from Nand flash/ SD Card / Internal memory

618件の閲覧回数
muralikrishna
Contributor I

In I.MX6 Quad processor, what are hardware pins to be used in the schematic for selecting boot options from NAND Flash / SD Card / Internal.

ラベル(1)
0 件の賞賛
返信
1 返信

517件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Murali

please look at SPF-27142  p.3, 9

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信