Hi community,
I'm trying to change desktop on weston.
And I modify weston.ini which is located under .config folder.
Below is my weston.ini content.
[core]
xwayland=true
#idle-time=0
#backend=drm-backend.so[shell]
type=desktop-shell.so
background-image=/usr/share/qt5/examples/quick/demos/rssnews/content/images/Technology.jpg
background-color=0x00000000[screensaver] path=/usr/lib/weston/weston-screensaver
duration=600[launcher]
icon=/usr/share/icons/Adwaita/24x24/apps/utilities-terminal-symbolic.symbolic.pn
path=/usr/bin/weston-terminal[launcher]
icon=/usr/share/icons/Adwaita/24x24/apps/preferences-system-sharing-symbolic.sym
path=/usr/bin/producttestingtool_qt5 -platform wayland
As you can see, I add [shell] and try to use Technology.jpg to be my new desktop.
But after I reboot the system, desktop did not change.
It still the default desktop.
How can I change it?
Thanks in Advanced!
Diego Adrian Cuevas 留言:
Hello,
Which i.MX and BSP are you using?
Best Regard,
Diego.
Thanks for your reply.
I'm using freescale released Yocto Project 2.0 with kernel 4.1.15 QT5.4.
And I using DISTRO "fsl-imx-wayland".
Is there anything I need to mention?
Solved, just fix with
[shell]
backgroung-color=0xffff0000
===============
Hi @diegoadrian
Same happend at
i.mx8qxp 5.15 fsl-imx-wayland
I add following change to weston.ini and nothing changed.
background-image=/home/root/driverExample/2022-07-26-170417.jpg
backgroung-color=0xffff0000
homescreen=/home/root/driverExample/2022-07-26-170417.jpg[libinput]
touchscreen_calibrator=false
transform=rotate-90
Also I try put weston.ini to following path, but still not work.
/etc/xdg/weston/weston.ini
~/.config/weston.ini
~/weston.ini
Any suggests?