Hi community,
I'm trying to change desktop on weston.
And I modify weston.ini which is located under .config folder.
Below is my weston.ini content.
[core]
xwayland=true
#idle-time=0
#backend=drm-backend.so[shell]
type=desktop-shell.so
background-image=/usr/share/qt5/examples/quick/demos/rssnews/content/images/Technology.jpg
background-color=0x00000000[screensaver] path=/usr/lib/weston/weston-screensaver
duration=600[launcher]
icon=/usr/share/icons/Adwaita/24x24/apps/utilities-terminal-symbolic.symbolic.pn
path=/usr/bin/weston-terminal[launcher]
icon=/usr/share/icons/Adwaita/24x24/apps/preferences-system-sharing-symbolic.sym
path=/usr/bin/producttestingtool_qt5 -platform wayland
As you can see, I add [shell] and try to use Technology.jpg to be my new desktop.
But after I reboot the system, desktop did not change.
It still the default desktop.
How can I change it?
Thanks in Advanced!
I am facing same issue in kernel version 5.10.9, yocto project 3.2
My weston.ini is not updating
i am copying to /etc/xdg/weston/
Thanks
Abhishek
hello may i know where is the weston.ini ,i want to remove the top bar,but i can not find the file。。
try: /etc/xdg/weston/weston.ini
thanks!
after modify weston.ini.
command: "systemctl restart weston"
reboot your system to apply
Hello,
Which i.MX and BSP are you using?
Best Regard,
Diego.
Diego Adrian Cuevas 留言:
Hello,
Which i.MX and BSP are you using?
Best Regard,
Diego.
Thanks for your reply.
I'm using freescale released Yocto Project 2.0 with kernel 4.1.15 QT5.4.
And I using DISTRO "fsl-imx-wayland".
Is there anything I need to mention?
Hello,
I apologize for the delay.
Can you please try to put the weston.ini file in the root directory and try to see if that works?
Best Regards,
Diego
Solved, just fix with
[shell]
backgroung-color=0xffff0000
===============
Hi @diegoadrian
Same happend at
i.mx8qxp 5.15 fsl-imx-wayland
I add following change to weston.ini and nothing changed.
background-image=/home/root/driverExample/2022-07-26-170417.jpg
backgroung-color=0xffff0000
homescreen=/home/root/driverExample/2022-07-26-170417.jpg[libinput]
touchscreen_calibrator=false
transform=rotate-90
Also I try put weston.ini to following path, but still not work.
/etc/xdg/weston/weston.ini
~/.config/weston.ini
~/weston.ini
Any suggests?