weston fails to start on imx8 mini when using MX8-DSI_OLED1A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

weston fails to start on imx8 mini when using MX8-DSI_OLED1A

1,907 次查看
leviriley
Contributor II

I am using the wayland imx-image-full image with chromium added
If I use the mipi hdmi dongle things work swimmingly and can verify chromium works

 

I tried: 
U-Boot > setenv fdt_file fsl-imx8mq-evk-dcss-rm67191.dtb
U-Boot > run bootcmd

however it fails on boot and manually starting weston does not succeed:

 
root@imx8mm-lpddr4-evk:~# weston --tty[1~7] --debug

Date: 2022-07-09 UTC
[01:56:51.289] weston 9.0.0
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: 9.0.0
[01:56:51.290] Command line: weston --tty[1~7] --debug
[01:56:51.290] OS: Linux, 5.15.5-lts-next+gc1084c2773fc, #1 SMP PREEMPT Mon Mar 7 20:03:59 UTC 2022, aarch64
[01:56:51.290] Using config file '/etc/xdg/weston/weston.ini'
WARNING: debug protocol has been enabled. This is a potential denial-of-service attack vector and information leak.
[01:56:51.290] Output repaint window is 16 ms maximum.
[01:56:51.290] Loading module '/usr/lib/libweston-9/drm-backend.so'
[01:56:51.295] initializing drm backend
[01:56:51.295] logind: failed to get session seat
[01:56:51.295] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[01:56:51.295] <stdin> not a vt
[01:56:51.295] if running weston from ssh, use --tty to specify a tty
[01:56:51.295] fatal: drm backend should be run using weston-launch binary, or your system should provide the logind D-Bus API.
[01:56:51.295] fatal: failed to create compositor backend
Internal warning: debug scope 'drm-backend' has not been destroyed.


0 项奖励
回复
1 回复

1,884 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The dtb of MX8-DSI_OLED1A is xxxx-rm67199.dtb

0 项奖励
回复