websocketd runtime crash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

websocketd runtime crash

444 次查看
tommy2402
Contributor I

Dear NXP Community,

we use i.MX7 processors in combination with Yocto Project (Release 5.2 (walnascar)).

Last years we used the community kernel [linux-fslc](https://github.com/Freescale/linux-fslc).

Since security requirements getting tighter, we decided to switch to official nxp kernel [linux-imx](https://github.com/nxp-imx/linux-imx) (lf-6.12.y).

Problem: Beside others, we use [websocketd](https://github.com/joewalnes/websocketd) with this example [yocto-recipe](https://layers.openembedded.org/layerindex/recipe/152495/) and it worked well with freescale linux-fslc (tested on different versions). Websocketd is mainly written in go.

When running linux-imx we observer sporadic crashes like:

runtime: s.allocCount= 991 s.nelems= 992
fatal error: s.allocCount != s.nelems && freeIndex == s.nelems

goroutine 121 gp=0x29465a8 m=3 mp=0x2839008 [running]:
runtime.throw({0x836e6b, 0x31})
runtime/panic.go:1101 +0x38 fp=0x284995c sp=0x2849948 pc=0x53c8a8

......

2025/07/17 10:10:14 http: panic serving 127.0.0.1:41334: runtime error: invalid memory address or nil pointer dereference
goroutine 72 [running]:
net/http.(*conn).serve.func1()
net/http/server.go:1947 +0xf0
panic({0x876cd8, 0xa535f8})
runtime/panic.go:792 +0x110


We don´t think that these are bugs inside the application (since it works well on linux-fslc - device tree and kernel config are the same).

Is there anything we missed during the switch over from linux-fslc to linux-imx (MMU, DMA, thread-model ...)?

Thanks in advance and best regards,

Tommy

标签 (4)
标记 (2)
0 项奖励
回复
1 回复

421 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello, 

I think you should go with the yocto community sice websocket works with the latest NXP release.

https://www.yoctoproject.org/community/mailing-lists/

 

Regards

 

0 项奖励
回复