we are not able to flash the image on I.MX8ULP using UUU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

we are not able to flash the image on I.MX8ULP using UUU

481 Views
Dhaval_Shiroya
Contributor I

Hello folks,

We have MCIMX8ULP-SOM and x-8ulp-acep-epd carrier board.

We are trying to flash pre-build Linux image downloaded from official site of NXP, but we are facing below error while flashing the image.

1:3 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -scanterm -f imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot -scanlimited 0x800000

It would be great, if anybody can help us.

0 Kudos
Reply
2 Replies

417 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @Dhaval_Shiroya 

 

You can refer to AN14120 for how to flash the image on i.MX8ULP.

danielchen_0-1745930139065.png

 

 

Regards

Daniel

 

0 Kudos
Reply

452 Views
AshutoshNama
Contributor III
0 Kudos
Reply