we are not able to flash the image on I.MX8ULP using UUU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

we are not able to flash the image on I.MX8ULP using UUU

591 次查看
Dhaval_Shiroya
Contributor I

Hello folks,

We have MCIMX8ULP-SOM and x-8ulp-acep-epd carrier board.

We are trying to flash pre-build Linux image downloaded from official site of NXP, but we are facing below error while flashing the image.

1:3 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -scanterm -f imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot -scanlimited 0x800000

It would be great, if anybody can help us.

0 项奖励
回复
2 回复数

527 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi @Dhaval_Shiroya 

 

You can refer to AN14120 for how to flash the image on i.MX8ULP.

danielchen_0-1745930139065.png

 

 

Regards

Daniel

 

0 项奖励
回复

562 次查看
AshutoshNama
Contributor III
0 项奖励
回复