wayland问题

cancel
Showing results for 
Search instead for 
Did you mean: 

wayland问题

1,893 Views
senli
Contributor II

大家好!

       我现在用的LinuxBSP 是3.14.52,CPU是imx6q.目前编译X11是没有问题,系统运行也正常。

       现在想编译wanyland,我看文档上说编译wayland是运行 bitbake fsl-image-weston

       但是我在source目录里面没有看到fsl-image-weston的   bb文件,所以也就没有办法编译。

        请高手指点下怎么编译wayland.

Labels (1)
7 Replies

671 Views
joanxie
NXP TechSupport
NXP TechSupport

$ DISTRO=fsl-imx-xwayland MACHINE=board_name source fsl-setup-release.sh –b build-xwayland
$ bitbake fsl-image-gui

This builds an Xwayland image without Qt 5. if you need qt5, use bitbake fsl-image-qt5

671 Views
senli
Contributor II

你好,我参考上面的命令重新编译了image,但是开机后显示了小企鹅的图标和启动进度条后,就黑屏了(背光是正常亮着的)。

没有看到桌面的界面。请看看是什么原因,是不是还有什么要配置的。

0 Kudos

671 Views
joanxie
NXP TechSupport
NXP TechSupport

try to use  "echo "number" > /sys/class/graphics/fb0/blank" , number = 0 or 1

0 Kudos

671 Views
senli
Contributor II

你好!

        这个命令是控制背光开启关闭的吧。

        我试了这个命令只是控制了背光亮和灭。

        我现在的问题是背光和显示驱动没有问题,背光一直亮着,小企鹅的图标和开机的进度都显示正常。

        就是没有桌面出来。应该是桌面没有跑起来。

0 Kudos

671 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mind uploading your log file and image to check? yes the command is for backlight, and did you try the demo image? the same issue?

0 Kudos

671 Views
senli
Contributor II

你好!

        请帮忙确认下3.14.52的BSP时候能支持wayland ?

0 Kudos

671 Views
senli
Contributor II

你好!

        下面是log信息,请帮忙看看。

        我没有用demo image测试,应为我们用的LCD屏是双通道的LVDS屏,和DOME板上的不一样,用demo image点不亮屏

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Mar 21 2017 - 19:38:27)

CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 55 C
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2(part 0) is current device
Net: Phy 1 not found
PHY reset timed out
FEC [PRIME]
Error: FEC address not set.

Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc2(part 0) is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
3645528 bytes read in 109 ms (31.9 MiB/s)
Booting from mmc ...
reading imx6q-sabresd.dtb
44733 bytes read in 19 ms (2.2 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x37a058 ]
## Flattened Device Tree blob at 18000000
Booting using the fdt blob at 0x18000000
Using Device Tree in place at 18000000, end 1800debc

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.52-1.1.0_ga+g5f6f0a5 (lisen@itas-softlinux) (gcc version 4.9.2 (GCC) ) #2 SMP PREEMPT Thu Mar 23 11:09:06 CST 2017
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
[ 0.000000] cma: CMA: reserved 320 MiB at 3c000000
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] PERCPU: Embedded 8 pages/cpu @ab722000 s8320 r8192 d16256 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096
[ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk3p2 rootwait rw
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 704216K/1048576K available (4334K kernel code, 207K rwdata, 1628K rodata, 208K init, 378K bss, 344360K reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xc0800000 - 0xff000000 (1000 MB)
[ 0.000000] lowmem : 0x80000000 - 0xc0000000 (1024 MB)
[ 0.000000] pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
[ 0.000000] modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
[ 0.000000] .text : 0x80008000 - 0x805dacd4 (5964 kB)
[ 0.000000] .init : 0x805db000 - 0x8060f080 ( 209 kB)
[ 0.000000] .data : 0x80610000 - 0x80643c20 ( 208 kB)
[ 0.000000] .bss : 0x80643c2c - 0x806a255c ( 379 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] L310 cache controller enabled
[ 0.000000] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x32070000, Cache size: 1024 kB
[ 0.000000] Switching to timer-based delay loop
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655765682ns
[ 0.000794] Console: colour dummy device 80x30
[ 0.000812] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.000826] pid_max: default: 32768 minimum: 301
[ 0.001001] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001015] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001696] CPU: Testing write buffer coherency: ok
[ 0.001962] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002026] Setting up static identity map for 0x10420148 - 0x104201a0
[ 0.061046] CPU1: Booted secondary processor
[ 0.061067] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.081050] CPU2: Booted secondary processor
[ 0.081070] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.101040] CPU3: Booted secondary processor
[ 0.101060] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.101162] Brought up 4 CPUs
[ 0.101192] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[ 0.101201] CPU: All CPU(s) started in SVC mode.
[ 0.101770] devtmpfs: initialized
[ 0.105308] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.105623] pinctrl core: initialized pinctrl subsystem
[ 0.105878] regulator-dummy: no parameters
[ 0.121929] NET: Registered protocol family 16
[ 0.130375] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.130846] cpuidle: using governor ladder
[ 0.130857] cpuidle: using governor menu
[ 0.130956] CPU identified as i.MX6Q, silicon rev 1.5
[ 0.131060] Use WDOG1 as reset source
[ 0.140038] syscon 20c8000.anatop: regmap [mem 0x020c8000-0x020c8fff] registered
[ 0.140366] vdd1p1: 800 <--> 1375 mV at 1100 mV
[ 0.140676] vdd3p0: 2625 <--> 3400 mV at 3000 mV
[ 0.140961] vdd2p5: 2000 <--> 2750 mV at 2400 mV
[ 0.141272] vddarm: 725 <--> 1450 mV at 1150 mV
[ 0.150351] vddpu: 725 <--> 1450 mV
[ 0.150672] vddsoc: 725 <--> 1450 mV at 1175 mV
[ 0.152738] syscon 20e0000.iomuxc-gpr: regmap [mem 0x020e0000-0x020e0037] registered
[ 0.155643] syscon 21bc000.ocotp-ctrl: regmap [mem 0x021bc000-0x021bffff] registered
[ 0.160720] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.160731] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.160943] imx6q-pinctrl 20e0000.iomuxc: no fsl,pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/imx6qdl-sabresd/enetirqgrp
[ 0.161192] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.176850] bio: create slab <bio-0> at 0
[ 0.178941] mxs-dma 110000.dma-apbh: initialized
[ 0.179713] usb_otg_vbus: 5000 mV
[ 0.179902] usb_h1_vbus: 5000 mV
[ 0.180101] wm8962-supply: no parameters
[ 0.180287] mipi_dsi_pwr_on: no parameters
[ 0.180497] sensor-supply: 3300 mV
[ 0.180873] SCSI subsystem initialized
[ 0.180990] usbcore: registered new interface driver usbfs
[ 0.181052] usbcore: registered new interface driver hub
[ 0.181163] usbcore: registered new device driver usb
[ 0.181312] usbphy_nop1.11 supply vcc not found, using dummy regulator
[ 0.181380] usbphy_nop2.12 supply vcc not found, using dummy regulator
[ 0.183097] i2c i2c-0: IMX I2C adapter registered
[ 0.184958] i2c i2c-1: IMX I2C adapter registered
[ 0.186310] i2c i2c-2: IMX I2C adapter registered
[ 0.186454] Linux video capture interface: v2.00
[ 0.186501] pps_core: LinuxPPS API ver. 1 registered
[ 0.186511] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.200396] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.220394] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.222171] Switched to clocksource mxc_timer1
[ 0.231954] NET: Registered protocol family 2
[ 0.232741] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.232830] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.232963] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.233098] TCP: reno registered
[ 0.233114] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.233154] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.233421] NET: Registered protocol family 1
[ 0.233846] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[ 0.234715] imx_busfreq busfreq.15: DDR medium rate not supported.
[ 0.235150] Bus freq driver module loaded
[ 0.236089] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.243931] fuse init (API version 7.22)
[ 0.244361] msgmni has been set to 2015
[ 0.246199] io scheduler noop registered
[ 0.246210] io scheduler deadline registered
[ 0.246386] io scheduler cfq registered (default)
[ 0.247740] backlight.25 supply power not found, using dummy regulator
[ 0.249241] ldb ldb.14: split mode
[ 0.249396] ldb ldb.14: split mode or dual mode, ignoring second output
[ 0.250043] mxc_sdc_fb fb.24: registered mxc display driver ldb
[ 0.282247] imx-ipuv3 2800000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 0.287983] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[ 0.288311] imx-sdma 20ec000.sdma: no event needs to be remapped
[ 0.288556] imx-sdma 20ec000.sdma: loaded firmware 3.2
[ 0.291460] imx-sdma 20ec000.sdma: initialized
[ 0.293015] pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
[ 0.293623] pfuze100-regulator 1-0008: FAB: 0, FIN: 0
[ 0.293635] pfuze100-regulator 1-0008: pfuze100 found.
[ 0.295134] SW1AB: 300 <--> 1875 mV at 1375 mV
[ 0.296465] SW1C: 300 <--> 1875 mV at 1375 mV
[ 0.298230] SW2: 800 <--> 3300 mV at 3300 mV
[ 0.298975] SW3A: 400 <--> 1975 mV at 1500 mV
[ 0.299701] SW3B: 400 <--> 1975 mV at 1500 mV
[ 0.300425] SW4: 800 <--> 3300 mV at 3150 mV
[ 0.301152] SWBST: 5000 <--> 5150 mV at 5000 mV
[ 0.301875] VSNVS: 1000 <--> 3000 mV at 3000 mV
[ 0.301999] VREFDDR: 750 mV
[ 0.302718] VGEN1: 800 <--> 1550 mV at 1500 mV
[ 0.303447] VGEN2: 800 <--> 1550 mV at 1500 mV
[ 0.304182] VGEN3: 1800 <--> 3300 mV at 2800 mV
[ 0.304917] VGEN4: 1800 <--> 3300 mV at 1800 mV
[ 0.305653] VGEN5: 1800 <--> 3300 mV at 3000 mV
[ 0.306391] VGEN6: 1800 <--> 3300 mV at 3300 mV
[ 0.306485] Serial: IMX driver
[ 0.306771] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 58, base_baud = 5000000) is a IMX
[ 1.086371] console [ttymxc0] enabled
[ 1.090635] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 59, base_baud = 5000000) is a IMX
[ 1.099754] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 60, base_baud = 5000000) is a IMX
[ 1.108806] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 61, base_baud = 5000000) is a IMX
[ 1.117847] 21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 62, base_baud = 5000000) is a IMX
[ 1.127803] [drm] Initialized drm 1.1.0 20060810
[ 1.132773] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[ 1.145885] brd: module loaded
[ 1.152779] loop: module loaded
[ 1.156445] CAN device driver interface
[ 1.160463] 2090000.can supply xceiver not found, using dummy regulator
[ 1.167890] flexcan 2090000.can: device registered (reg_base=c0a00000, irq=142)
[ 1.175497] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.182035] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 1.188363] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 1.199653] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 1.204589] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 1.222199] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 1.228356] hub 1-0:1.0: USB hub found
[ 1.232151] hub 1-0:1.0: 1 port detected
[ 1.239839] ci_hdrc ci_hdrc.1: doesn't support gadget
[ 1.244953] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 1.249861] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[ 1.272197] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 1.278302] hub 2-0:1.0: USB hub found
[ 1.282093] hub 2-0:1.0: 1 port detected
[ 1.286967] snvs_rtc 20cc034.snvs-rtc-lp: can't get snvs-rtc clock
[ 1.293508] snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
[ 1.301900] i2c /dev entries driver
[ 1.306576] mxc_v4l2_output v4l2_out.27: V4L2 device registered as video16
[ 1.313625] mxc_v4l2_output v4l2_out.27: V4L2 device registered as video17
[ 1.321074] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
[ 1.329597] sdhci: Secure Digital Host Controller Interface driver
[ 1.335947] sdhci: Copyright(c) Pierre Ossman
[ 1.340315] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.347052] mmc3: no vqmmc regulator found
[ 1.351168] mmc3: no vmmc regulator found
[ 1.392191] mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
[ 1.400126] Galcore version 5.0.11.33433
[ 1.477582] mmc3: BKOPS_EN bit is not set
[ 1.493618] mmc3: new high speed DDR MMC card at address 0001
[ 1.500550] mmcblk3: mmc3:0001 MMC08G 7.26 GiB
[ 1.505875] mmcblk3boot0: mmc3:0001 MMC08G partition 1 16.0 MiB
[ 1.512564] mmcblk3boot1: mmc3:0001 MMC08G partition 2 16.0 MiB
[ 1.519172] mmcblk3rpmb: mmc3:0001 MMC08G partition 3 128 KiB
[ 1.527802] mmcblk3: p1 p2
[ 1.535026] mmcblk3boot1: unknown partition table
[ 1.543227] mmcblk3boot0: unknown partition table
[ 1.602343] usb 2-1: new high-speed USB device number 2 using ci_hdrc
[ 1.968335] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 1.976691] mxc_vpu 2040000.vpu: VPU initialized
[ 1.982403] NET: Registered protocol family 26
[ 1.986998] TCP: cubic registered
[ 1.990325] NET: Registered protocol family 17
[ 1.994823] can: controller area network core (rev 20120528 abi 9)
[ 2.001089] NET: Registered protocol family 29
[ 2.005587] can: raw protocol (rev 20120528)
[ 2.009869] can: broadcast manager protocol (rev 20120528 t)
[ 2.015561] can: netlink gateway (rev 20130117) max_hops=1
[ 2.021227] 8021q: 802.1Q VLAN Support v1.8
[ 2.027438] VGEN3: disabling
[ 2.030792] VGEN2: disabling
[ 2.034159] VGEN1: disabling
[ 2.037497] SWBST: disabling
[ 2.040390] SW4: disabling
[ 2.043162] sensor-supply: disabling
[ 2.046765] mipi_dsi_pwr_on: disabling
[ 2.050535] wm8962-supply: disabling
[ 2.054137] regulator-dummy: disabling
[ 2.058214] snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:11:27 UTC (687)
[ 2.314546] EXT4-fs (mmcblk3p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.322754] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.333280] devtmpfs: mounted
[ 2.336577] Freeing unused kernel memory: 208K (805db000 - 8060f000)
INIT: version 2.88 booting
Starting udev
[ 3.041755] udevd[133]: starting version 182
[ 3.525295] usb-storage 2-1:1.0: USB Mass Storage device detected
[ 3.532507] DBG sensor data is at 7f01c218
[ 3.566118] scsi0 : usb-storage 2-1:1.0
[ 3.570598] usbcore: registered new interface driver usb-storage
[ 3.959958] ERROR: v4l2 capture: slave not found!
[ 4.563324] scsi 0:0:0:0: Direct-Access Kingston DataTraveler 3.0 PQ: 0 ANSI: 6
[ 4.587667] sd 0:0:0:0: [sda] 30218842 512-byte logical blocks: (15.4 GB/14.4 GiB)
[ 4.595649] sd 0:0:0:0: [sda] Write Protect is off
[ 4.600896] sd 0:0:0:0: [sda] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA
[ 4.615413] sda: sda1
[ 4.620272] sd 0:0:0:0: [sda] Attached SCSI removable disk
[ 4.872317] random: nonblocking pool is initialized
[ 5.300130] FAT-fs (sda1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 10.790516] EXT4-fs (mmcblk3p2): re-mounted. Opts: (null)
bootlogd: cannot allocate pseudo tty: No such file or directory
/etc/rcS.d/S38itas-can-bus.sh: line 7: /usr/share/itas-qt5-demo-1.0/itas-qt5-demo-1.0: No such file or directory
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1729: No soundcards found...
Thu Mar 23 07:45:50 UTC 2017
INIT: Entering runlevel: 5
Starting system message bus: resize: can't open terminal /dev/tty
Starting Xserver
resize: can't open terminal /dev/tty
Unknown username "xuser" in message bus configuration file
dbus.
Starting Connection Manager
resize: can't open terminal /dev/tty
rm: cannot remove '/var/log/weston.log': No such file or directory
openvt: Using VT /dev/tty1
Starting Dropbear SSH server: Generating key, this may take a while...
Public key portion is:
ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQDF89m7u1MjlqUVdB4zczCJJTeVwTWLZ2j4jEm2l/0vqIq+MGp488/L+UG+/uTnMNIBcLEZHVs/5J3p6sKnNNE6Cx0U4t+gBgvmBuPN9Q1FI+2Us8jDbTqZmHwN/kWwfMAL5GbyiqRM0iWUqyYpYSzOdVB/KJGSfVki/WnjlBB0tDVhgb9xnUEIuEM2KLWDdLIq+00iW6A4oXRTUsColez6ul/0fJCL9CNGVuUvhC6pZUvBRdl5ktTaXfMipERAZslo5r4KOjjDqZoWkmLmM0+hxsN9caf41mGOBii1cHwil+bOMPdW8XRwHvKNyTd+TE05u8TAflDi6qxCBsRuOibb root@imx6qsabresd
Fingerprint: md5 59:9e:a3:3e:a1:25:3f:21:a3:e2:51:9b:37:ed:b0:0a
dropbear.
Starting rpcbind daemon...rpcbind: cannot create socket for udp6
rpcbind: cannot create socket for tcp6
done.
starting statd: done
Starting advanced power management daemon: No APM support in kernel
(failed.)
NFS daemon support not enabled in kernel
Starting syslogd/klogd: done
[ ok ]rting Avahi mDNS/DNS-SD Daemon: avahi-daemon
Starting Telephony daemon
Starting Linux NFC daemon
Starting OProfileUI server
resize: can't open terminal /dev/tty
Running local boot scripts (/etc/rc.local).

Freescale i.MX Release Distro 3.14.52-1.1.0 imx6qsabresd /dev/ttymxc0

imx6qsabresd login:

0 Kudos