vpu jpeg decoder successfully, but can't get output YUV data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vpu jpeg decoder successfully, but can't get output YUV data

Jump to solution
2,360 Views
moon
Contributor I

I use vpu to decode jpeg,  some code as below, after vpu_DecGetOutputInfo call successfully, I always can't get any decoded YUV data from frame buffer indicated by outInfo.indexFrameDisplay. platform is i.mx53 and linux. data of frame buffer are always 0s. indexFrameDisplay and indexFrameDecoded always 0.

// get output after decode code snippet

retVal = vpu_DecGetOutputInfo(pObj->handle, &outInfo);

if(retVal != RETCODE_SUCCESS)

{

  printf("vpu_DecGetOutputInfo failed: %d\n", retVal);

  exit(1);

}

if(outInfo.indexFrameDisplay != -1 && outInfo.indexFrameDisplay != -2 && outInfo.indexFrameDisplay != -3  && outInfo.prescanResult > 0 && outInfo.indexFrameDisplay >= 0)

  {

  picture = (AVFrame *)data;

  startFrameAddr = pObj->frame_buffer_desc[outInfo.indexFrameDisplay].virt_uaddr;

  picture->data[0] = (char *)startFrameAddr;

  picture->data[1] = (char *)(startFrameAddr + pObj->width * pObj->height);

  picture->data[2] =(char *)(picture->data[1] + pObj->width/2 * pObj->height/2);

  picture->linesize[0] = pObj->width;

  picture->linesize[1] = pObj->width / 2;

  picture->linesize[2] = pObj->width / 2;

  picture->height = pObj->height;

  picture->width = pObj->width;

}

 

// open decoder code snippets

  memset(&openParam, 0, sizeof(DecOpenParam));

  openParam.bitstreamBuffer = pObj->bitstream_mem_desc.phy_addr;

  openParam.bitstreamBufferSize = pObj->bitstream_mem_desc.size;

  openParam.bitstreamFormat = STD_MJPG;

  openParam.filePlayEnable = 0;

  openParam.dynamicAllocEnable = 0;

  if(vpu_DecOpen(&pObj->handle, &openParam) != RETCODE_SUCCESS)

  {

  printf("decoder open failure \n");

  exit(1);

  }

Labels (3)
1 Solution
1,874 Views
miloszlazurek
Contributor I

I had similar issues while working on I.MX.6 - Be sure to enable the ROTATOR feature when decoding JPEG if not doing it already. Refer to the freescale example decoder (dec.c) to see how it is done.

View solution in original post

0 Kudos
Reply
2 Replies
1,875 Views
miloszlazurek
Contributor I

I had similar issues while working on I.MX.6 - Be sure to enable the ROTATOR feature when decoding JPEG if not doing it already. Refer to the freescale example decoder (dec.c) to see how it is done.

0 Kudos
Reply
1,874 Views
prabhurammuruga
Contributor I

May I know where I could get the freescale example decoder ?

Search on freescale website did not help,

I am working on iMX53 , trying to use the VPU for jpeg decoding for a sample gallery application.

0 Kudos
Reply