v4l2 supportted format for 10 bit monochrome

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

v4l2 supportted format for 10 bit monochrome

1,227 Views
muralikrishnant
Contributor I

Dear sir;

      we interfaced 10 bit monochrome parallel image sensor  with imx6 and we had doubt about format supported by v4l2 capture so please provide the guidance and provide the sample driver

0 Kudos
Reply
1 Reply

1,076 Views
igorpadykov
NXP Employee
NXP Employee

Hi Muralikrishnan

what i.MX6 used in the case (full part number), in general one can look at

L4.1.15 BSP release, there is ov5647_mipi driver :drivers/media/platform/mxc/subdev/ov5647_mipi.c.

please check Linux Documentation on

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply