uuu with VirtualBox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uuu with VirtualBox

1,543件の閲覧回数
roni
Contributor I

I'm using UUU version 1.5.201 to flash an iMX93. When running this process within VirtualBox, the initial flashing stage completes without error. However, the second stage consistently times out. I am seeing console output (indicated by dots) from the device. What steps can I take to troubleshoot and resolve this timeout problem?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,521件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @roni 

I hope you are doing very well.

 

Could you please try in a PC host out of VirtualBox environment?

Maybe VirtualBox is adding an USB filter or something like that.

The first stage is SDP over USB, but then involves fastboot, flash bootloader, Linux, etc.

 

Please try to use a PC host to flash your device.

 

Best regards,

Salas.

0 件の賞賛
返信

1,490件の閲覧回数
roni
Contributor I

Hi

I am using the command "uuu -d -v -b emmc_all ..boot ...rootfs.wic
I case I am running from Linux Host , the UUU program the IMX93 
in case of running from Virtual box  . it stack at

"Starting download of 16776232 bytes

..........................................................................
....................................................."
 
 
 
see all the device terminal:
U-Boot SPL 2024.04-compulab+g2d2dd77f15+p0 (Feb 11 2025 - 09:18:39 +0000)
SOC: 0xa1009300
LC: 0x2040010
DDRINFO: applied cfg: Micron 2048MB @ 3733 MHz
M33 prepare ok
Normal Boot
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x88000000, size 416
Download 1713152, Total size 1714176
NOTICE:  TRDC init done
NOTICE:  BL31: v2.10.0 (release):android-15.0.0_1.0.0-rc3-0-g1b27ee3ed
NOTICE:  BL31: Built : 08:52:12, Nov  4 2024
 
 
U-Boot 2024.04-compulab+g2d2dd77f15+p0 (Feb 11 2025 - 09:18:39 +0000)
 
CPU:   NXP i.MX93(52) Rev1.1 A55 at 1700 MHz at 40C
 
Model: CompuLab MCM-i.MX93 board
DRAM:  2 GiB
Core:  207 devices, 29 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from nowhere... OK
[*]-Video Link 0 (1024 x 600)
[0] lcd-controller@4ae30000, video
[1] lvds-channel@0, display
[2] lvds0_panel, panel
In:    serial
Out:   serial
Err:   serial
 
BuildInfo:
  - ELE firmware version 2.0.0-64d8ef47
 
MMC: no card present
board_late_init [ 0x7e000000 ]
UID: 0x60b967d6 0x1f470be5 0x62cda391 0x2abb2d40
Detect USB boot. Will enter fastboot mode!
Net:   eth1: ethernet@42890000, eth0: ethernet@428a0000
Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for mfgtools
, using default environment
 
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot auto; fi;
Hit any key to stop autoboot:  0 
 
## Checking Image at 83800000 ...
Unknown image format!
Run fastboot ...
auto usb 0
UID: 0x60b967d6 0x1f470be5 0x62cda391 0x2abb2d40
Detect USB boot. Will enter fastboot mode!
flash target is MMC:1
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 1 not supported
Detect USB boot. Will enter fastboot mode!
flash target is MMC:0
switch to partitions #0, OK
mmc0(part 0) is current device
Detect USB boot. Will enter fastboot mode!
Starting download of 16776232 bytes
..........................................................................
.....................................................
 
 

 

0 件の賞賛
返信