uuu stuck on 99%

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uuu stuck on 99%

2,076 Views
allonli
Contributor II

IMX8MPLUS platform

DDR stress test pass successfully.

build flash.bin standalone

"uuu.exe -b emmc flash.bin" stuck on 99%, UART no log output.

is there any debug method for such situation? 

0 Kudos
Reply
7 Replies

2,072 Views
allonli
Contributor II

ps:add -V parameters, it show error below:

99%libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 设备没有连接。
1:11>Okay (1.libusb: warning [winusb_get_device_list] could not detect installation state of driver for 'USB\VID_1FC9&PID_0146\6&17382A9&0&1': [3758096907] 设备实例不在硬件树中。

0 Kudos
Reply

2,066 Views
igorpadykov
NXP Employee
NXP Employee

Hi Allon

 

one can recheck if uuu version is compatible with flash.bin,

recommended uuu version is described in Release Notes document of each bsp:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 Kudos
Reply

2,058 Views
allonli
Contributor II

Hi,Igor,

  yes, I use the uuu version as release note described, but same erro.

libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 设备没有连接。

 

0 Kudos
Reply

2,045 Views
igorpadykov
NXP Employee
NXP Employee

one can try on other computer.

 

Best regards
igor

0 Kudos
Reply

2,040 Views
allonli
Contributor II

yes, have tried.

and also test under Ubuntu system, the same result, but no "winusb" error message even add -V option, just stuck on 99%.

0 Kudos
Reply

2,033 Views
igorpadykov
NXP Employee
NXP Employee

could you try to reproduce issue on i.MX8M Plus EVK.

 

Best regards
igor

 

 

0 Kudos
Reply

2,007 Views
allonli
Contributor II

Hi, Igor,

Sorry,It should not be a uuu tools issue, cannt reproduce on EVK.

It may be customerize hardware or software problem, when stuck here, what's the possible problem, or how to debug it?

thanks a lot.

0 Kudos
Reply