uuu imx8mq flash to emmc loop

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uuu imx8mq flash to emmc loop

371 次查看
munchiis
Contributor I

I am having issues with uuu when attempting to flash to emmc on a custom board. I am using windows 10 and have been previously flashing without a problem, but now my log seems to be stuck in a loop and only repeats the output below. Any one have any idea as to why?

New USB Device Attached at 2:2
2:2>Start Cmd:SDPV: delay 1000 
2:2>Okay (1.001s)
2:2>Start Cmd:SDPV: write -f u-boot-imx8mq-evk-uuu.imx.link -skipspl 

3%
6%
10%
13%
17%
20%
24%
27%
31%
34%
38%
41%
45%
48%
52%
55%
59%
62%
66%
69%
73%
76%
80%
83%
87%
90%
93%
97%
100%2:2>Okay (1.39s)
2:2>Start Cmd:SDPV: jump 

0%
6400%2:2>Okay (0.103s)
New USB Device Attached at 2:2
2:2>Start Cmd:SDP: boot -f u-boot-imx8mq-evk-uuu.imx.link 

14%
28%
43%
57%
72%
86%
100%
0%
6400%
0%
6400%2:2>Okay (0.565s)
New USB Device Attached at 2:2
2:2>Start Cmd:SDPV: delay 1000 
2:2>Okay (1.001s)
2:2>Start Cmd:SDPV: write -f u-boot-imx8mq-evk-uuu.imx.link -skipspl 

 

 

 

 

0 项奖励
0 回复数