uuu download images for imx8qxp mek

cancel
Showing results for 
Search instead for 
Did you mean: 

uuu download images for imx8qxp mek

3,892 Views
zhaocq
Contributor II

Could you give me some advice on android 9.0 download imx8qxp mek?

I want to download images on imx8qxp mek using uuu tool, the error is Wait for Known USB Device Appear...

(1) SW2 set 0001 serial download mode.

(2) Connecting J39 to PC USB by a USB OTG cable.

(3) Connecting J10(usb type c) to PC USB by a USB 3.0 cable.

(4) Power on I.MX8qxp mek board via J9

E:\imx8qxp_android9\android_p9.0.0_2.0.0-ga_image_8qmek>uuu_imx_android_flash.bat -f imx8qxp -a -e
This script is validated with uuu 1.2.91 version, please align with this version.
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash u-boot-imx8qxp.imx to the partition of bootloader0
generate lines to flash dtbo-imx8qxp.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8qxp.img to the partition of vbmeta_a
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.135-0-gacaf035

Your console don't support VT mode, fail back to verbose mode
Build in config:
        Pctl     Chip            Vid     Pid     BcdVersion
        ==================================================
        SDPS:    MX8QXP          0x1fc9  0x012f  [0x0002..0xffff]
        SDPS:    MX8QM           0x1fc9  0x0129  [0x0002..0xffff]
        SDPS:    MX28            0x15a2  0x004f
        SDPS:    MX815           0x1fc9  0x013e
        SDP:     MX7D            0x15a2  0x0076
        SDP:     MX6Q            0x15a2  0x0054
        SDP:     MX6D            0x15a2  0x0061
        SDP:     MX6SL           0x15a2  0x0063
        SDP:     MX6SX           0x15a2  0x0071
        SDP:     MX6UL           0x15a2  0x007d
        SDP:     MX6ULL          0x15a2  0x0080
        SDP:     MX6SLL          0x1fc9  0x0128
        SDP:     MX7ULP          0x1fc9  0x0126
        SDP:     MXRT106X        0x1fc9  0x0135
        SDP:     MX8MM           0x1fc9  0x0134
        SDP:     MX8MQ           0x1fc9  0x012b
        SDPU:    SPL             0x0525  0xb4a4  [0x0000..0x04ff]
        SDPV:    SPL1            0x0525  0xb4a4  [0x0500..0x9998]
        SDPU:    SPL             0x0525  0xb4a4  [0x9999..0x9999]
        FBK:                     0x066f  0x9afe
        FBK:                     0x066f  0x9bff
        FB:                      0x0525  0xa4a5
        FB:                      0x18d1  0x0d02
Wait for Known USB Device Appear...

11 Replies

2,552 Views
zhaocq
Contributor II

i use win7  when detect the devices, i need to pull out then pull in the type C wire. linux don't need to do it. you can try it.

0 Kudos

2,552 Views
zhaocq
Contributor II

win7 enviroment , i can download images successfully. Thanks

0 Kudos

2,552 Views
joanxie
NXP TechSupport
NXP TechSupport

my win10 doesn't work either, so I download under linux by "sudo ./uuu_imx_android_flash.sh -f imx8mq -a -e" successfully

0 Kudos

2,552 Views
zhaocq
Contributor II

 imx8qxp mek have three usb interface:usb debug, usb type c and usb otg. i want to enter serial download mode. which interface i shoud connect? what devices can be see in "device manager" ?

0 Kudos

2,552 Views
joanxie
NXP TechSupport
NXP TechSupport

use type C for downloading, you should find new devices under "Human Interface Device" of device manager

0 Kudos

2,552 Views
zhaocq
Contributor II

should i install the fastboot tool? after output the following log, it stop

1:6>Start Cmd:SDPS: boot -f u-boot-imx8qm-mek-uuu.imx.link
100%1:6>Okay

0 Kudos

2,552 Views
joanxie
NXP TechSupport
NXP TechSupport

it should be USB compatibility issue, you can try to use another USB port or try to use usb hub to connect your board

0 Kudos

2,552 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the settings in the board, for serial download mode, should be 1000, not 0001 pls double check it

0 Kudos

2,552 Views
zhaocq
Contributor II

Thanks for your reply, maybe just understood differently, should be from 4 to 1, is 0001

0 Kudos

2,552 Views
joanxie
NXP TechSupport
NXP TechSupport

if you set the SW2 correctly, pls check if your "device manager" detect your board or not, it seems your PC doesn't detect your board

0 Kudos

2,552 Views
zhaocq
Contributor II

Thanks, Could you show "device manager " detect device successfully , we can see what device? I don't know wether my imx8qxp mek using ic type PIMX8QX6AVLFZAA , i can not detect device. i will chang ic to PIMX8QX6AVLFZAB

0 Kudos